1112409_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1112409_en-US

1112409_en-US

How to use LPUART to RS485 on the i.MXRT1050

Recently, we often encounter customers using i.MXRT for RS485 communication. Mostly the problem of receiving and sending direction conversion in the process of using. Taking iMXRT1050 and SN65HVD11QDR as examples, The document introduces the LPUART to RS485 circuit and the method of transceiver control. The working principle is as follows:

pastedImage_1.png

LPUART TXD: Transmit Data

LPUART RXD: Receive Date

LPUART RTS_B: Request To Send

 

The main control methods are as follows:

1  Use TXD signal line to do hardware automatic transceiver control

pastedImage_2.png

According to the UART protocol, when the line is idle, TX is logic high. After the NOT gate, the LOW level is added to the direction control terminal, so when the UART is not  transmitting data, RS485 is in the state of receiving data.

2   Use GPIO control & LPUART_RTS

More detailed information, users can refer to the link:

https://www.nxp.com/docs/en/application-note/AN12679.pdf

pastedImage_4.png

Note: Using GPIO control, software needs to judge the timing of receiving and sending. If the control is not good, it is easy to lose data. In order to control it well, the software must respond to TX FIFO "empty" interrupt, or query the sending status register, and accurately grasp the control opportunity, so as to ensure that there is no error in sending and receiving.

Combined with the above methods, some customers are using the following control:

pastedImage_5.png

pastedImage_6.png

Best Regards

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-19-2025 11:08 AM
更新者: