1112383_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1112383_en-US

1112383_en-US

Datapath Software Acceleration using DPAA 2.0

This demo shows AIOP based data path offload for some of the popular Network Functions: IP Forward, IPSec, Netflow and Open Flow

 

 

Features:

  • The Data path offload software is 'C' program running in the AIOP and provides control interface at the GPP for integrating with the GPP based control stack.
  • The demonstration shows functionality of the above mentioned popular network applications live in the pedestal.
  • Performance demonstration of the above mentioned popular network applications using remote setup.
  • This implementation uses AIOP hardware accelerators – Table Lookup Unit, Statistics Engine,Timer Manager, Security Engine, Parser, CDMA/FDMA.

 

_______________________________________________________________________________________________________

 

Featured NXP Products:

_______________________________________________________________________________________________________

 

 

N09

Communications Infrastructure
Tags (1)
No ratings
Version history
Last update:
‎11-19-2025 06:01 AM
Updated by: