1108628_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1108628_en-US

1108628_en-US

Example S32K144 LPIT DMA LPSPI

********************************************************************************************
* Detailed Description:
* LPIT_ch0 triggers DMA_ch0 periodically (1ms).
* Every trigger starts a minor DMA loop (8 bytes) transfer to the LPSPI1 TX FIFO.
* There are 8 minor loops per one major loop (64 bytes in 8ms).
* LPSPI1 sends two 32bit frames every 1ms.

* LPSPI1 RX data are masked, they are not stored in the RX FIFO.
* ------------------------------------------------------------------------------
* Test HW: S32K144EVB-Q100
* MCU: S32K144 0N57U
* Debugger: S32DS 2.2, OpenSDA
* Target: internal_FLASH
********************************************************************************************

标记 (1)
无评分
版本历史
最后更新:
‎11-19-2025 03:12 AM
更新人: