1107719_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1107719_en-US

1107719_en-US

CodeWarrior for MCU v10.6 New Features<meta http-equiv="Content-Type" content="text/html; charset=utf-8" />

On April 2, 2014, Freescale released CodeWarrior for MCU v10.6( CW10.6 for short).

www.freescale.com/cwmcu10.

The CW10.6 platform integrates Freescale ColdFire ® , ColdFire+, DSC, Kinetis, Qorivva, RS08, S08 and S12Z development tools .

Like other previous versions of CW10 , CW10.6 is available for download in two versions:

  1. Online installation version ( 432M The downloaded installation package contains the core tools of CW MCU v10.6. Other installation packages need to be downloaded while being installed. This requires that the computer you are installing on can access the Internet and the speed is fast enough. In view of the general network conditions in mainland China, I do not recommend using it.
  2. Offline installation version ( 1.37GB The downloaded installation package includes CW All installation files of MCU v10.6. Even if the computer where the installation is done cannot access the Internet, it can still be installed and used normally.

Note: CW10.6 is an independent and complete version. CW10.6 can be installed independently on a computer that already has an older version installed. However, direct upgrade from the old version to the new version is not supported.

 

Compared with CW10.5 , CW10.6 adds support for the following products:

  • Kinetis E Series : MKE04Z8, MKE04Z64, MKE04Z128, MKE06Z64, MKE06Z128
  • Kinetis KEA family : SKEAZN16, SKEAZN32, SKEAZN64, SKEAZ128
  • Kinetis K 系列: MK24FN1M0, MK63FN1M0, MK64FX512, MK64FN1M0
  • Kinetis V Series : MKV10Z16, MKV10Z32
  • S08: HCS908RN8, HCS908RN16, HCS908RN32, HCS908RN48, HCS908RN60, HCS908RNA2, HCS908RNA4, HCS908RNA8, HCS908RNA16, HCS908RNA32, HCS908RNA48, HCS908RNA60
  • S12Z: MC9S12ZVC64, MC9S12ZVC128, MC9S12ZVC192, MC9S12ZVHY32

 

 

CW10.6 has upgraded the support for the following chips:

  • DSC: MC56F844xx, MC56F845xx, MC56F847xx
  • Kinetis E Series : MKE02Z16, MKE02Z32, MKE02Z64 (40MHz)
  • S12Z: MC9S12ZVFP64, MC9S12ZVHY64

 

New features:

  • For S12Z series chips, added support for 64bit 'long long' type and floating point
  • For Kinetis V series, supports square root operation and hardware division instructions
  • Added support for P&E Cyclone Universal [FX]

 

 

Use and upgrade of CW10.6 license :

  • The license of CW10.5 can be used in CW10.6.
  • But older versions of the license (ie 10.0, 10.1, 10.2, 10.3, 10.4) cannot be used with CW10.6. You need to purchase an upgrade from Freescale to upgrade the license .

 

 

Compatibility issues between MQX and CW10 :

  1. 1. MQX3.8 supports CW10.1 but not CW10.6.
  2. 2. MQX3.8.1 supports CW10.2 but not CW10.6.
  3. 3. MQX 4.0 is designed for CW10.2 and CW10.3 and has been tested on CW10.6 .
  4. 4. MQX 4.0.1 is designed for CW10.4 and has been tested on CW10.6.
  5. 5. MQX 4.0.2 is designed for CW10.4 and CW10.5 and has been tested on CW10.6.
  6. 6. MQX 4.1 is designed for CW10.5 and has been tested on CW10.6.
  7. 7. CW10.6 integrates MQX Lite RTOS. Supports Kinetis L and Kinetis K series
  8. 8. CW10.6 integrates the MQX Task Aware debugger, supporting debugging of MQX and MQX Lite
General
Tags (1)
No ratings
Version history
Last update:
‎01-05-2026 11:38 AM
Updated by: