1107440_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1107440_en-US

1107440_en-US

Accelerometer: MMA865x Breakout Board

Hi,

The MMA865x, 3-axis, 10-bit/12-bit accelerometer that has industry leading performance in a small 2 x 2 x 1 mm DFN package. This accelerometer is packed with embedded functions that include flexible user-programmable options and two configurable interrupt pins. Overall power savings is achieved through inertial wake-up interrupt signals that monitor events and remain in a low-power mode during periods of inactivity.

Here is a Render of the MMA865x Breakout- Board downloaded from OSH park:

PCB Render.png

Layout Design for this board:

Layout Render.png

In the attachments section, you can find the Schematic Source File (SCH), Schematic PDF File, Layout Source File (BRD), Gerber Files (GTL, GBL, GTS, GBS, GTO, GBO, GKO, XLN) and BOM files.

If you're interested in more designs like this breakout board for other sensors, please go to Freescale Sensors Breakout Boards Designs – HOME

Accelerometers
Tags (1)
No ratings
Version history
Last update:
‎02-05-2026 03:44 AM
Updated by: