1104163_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1104163_en-US

1104163_en-US

What to do if you fail a course at an Australian university<meta http-equiv="Content-Type" content="text/html; charset=utf-8" />

What to do if you fail a course in an Australian university? Contact QQ1252839746. You will be expelled from school for cheating, low GPA, or receive an academic warning. The final scores of Australian universities for 2018 S1 have been released one after another. When you get the scores, some people will inevitably feel frustrated. They didn’t take the exam for the content they reviewed, and they didn’t review the content for the exam, so they failed some subjects as expected...

Australian universities have always been lenient in admission and strict in graduation! With the release of grades, students are asking what to do if they fail a course. Let's learn how to deal with different situations of failing a course!

Less than or equal to 50% of failed subjects in the same semester

What does it mean to fail less than or equal to 50% of the subjects? The curriculum of each university is 4 courses per semester. If you fail 1-2 courses in a semester, but have not double failed (failed a course more than twice in a row), the school will not take any action against you. You must strive to pass all 4 courses in the next semester to make up for it!

The number of failed subjects in the same semester is greater than or equal to 50%.

Greater than or equal to 50% means that if you fail more than 2 courses in a semester, the school will generally take the first action and send you a warning letter!

School attendance is less than 80%

This has nothing to do with failing a course, but it is very important. If students have an attendance rate of less than 80% during a semester due to various reasons, and there is no reasonable reason for this low attendance rate, the school will first warn you and ask for an explanation. If the reason is not accepted by the school, the school is also qualified to report you to the Immigration Bureau, and the Immigration Bureau may cancel your visa based on the situation.

Study hard but still fail the exam

If you are a student who works very hard but still cannot control the situation and fails the exam, you should face your problem as soon as possible and summarize the reasons why you failed the exam. It may be because your major is not suitable, your learning ability is not good enough, or there are differences between your learning philosophy and the school... The most important thing for these students is to face their situation and consider transferring schools or changing majors.

警告信解释

When you unfortunately receive a dismissal warning letter, the quality of the written explanation is very important.

First, explain the reasons you have listed. They must be uncontrollable factors that lead to poor academic performance. Then express your firm belief that you can complete your studies and list the reasons. Finally, carefully plan how to overcome difficulties and work hard to improve your grades.

If you use health reasons as the reason, you must prepare supporting materials, such as a doctor's certificate, and submit them together. After accepting the application, the school will decide that it is necessary to hold a hearing, and will give an explanation after the hearing.

Regarding transferring schools, I need to remind you that if you are expelled from a public university, you will not be able to transfer to other public universities to continue your studies, and can only transfer to various private universities or colleges. However, you can start preparing for the transfer immediately after receiving a warning letter from the school and apply for the transfer before the expulsion procedure officially begins.

If you apply for transfer before completing 6 months of study, you will first need to obtain an offer from the school you want to transfer to, and then apply for a Release letter from your current school. Your current school will review your application based on the transfer policy and procedures, and then decide whether to issue a Release letter.

If you have been studying at the main school for more than six months, the school will generally agree to the student's transfer application.

In addition to the expensive tuition fees, failing a course in Australia may also result in forced expulsion and cancellation of your student visa, and you may not be allowed to enter Australia for three years, so you must be cautious about every exam. Australian universities can change grades if you fail a course (Q1252839746) and modify GPA scores if you fail a course to solve problems such as expulsion.

General
Tags (1)
No ratings
Version history
Last update:
‎01-05-2026 08:52 AM
Updated by: