1103412_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1103412_en-US

1103412_en-US

Example MPC5744P eTimer CTU ADC synchronization GHS614

********************************************************************************

* Detailed Description:

*

*

* This example shows synchronization between eTimer, CTU and ADC modules.

* The eTimer0 module timer 2 is initialized to generate PWM signal, and rising edge

* of this signal is used to generate trigger signal for CTU module. The CTU module

* use one command list with 4 ADC_0 channels. Single conversion mode is used,

* so ADC0 ch0, ch1, ch2 and ch3 are sampled.

* ------------------------------------------------------------------------------

* Test HW:  MPC57xx

* Maskset:  1N65H

* Target :  internal_FLASH

* Fsys:     200 MHz PLL with 40 MHz crystal reference

*

* EVB connection:

*

* P8.1  - A[0]  .. GPIO output, used to see CTU-ADC ISR period

* P9.1     - B[7]  .. ADC0 AN[0] input

* P9.2     - B[8]  .. ADC0 AN[1] input

* P16.4 - I[3] .. CTU0 EXT TRG output

*

* see CTU0 EXT TRG output signal (toggle on each trigger) on P16.4 with respect of eTimer PWM signals.

*

********************************************************************************

********************************************************************************

* Detailed Description:

*

*

* This example shows synchronization between eTimer, CTU and ADC modules.

* The eTimer0 module timer 2 is initialized to generate PWM signal, and rising edge

* of this signal is used to generate trigger signal for CTU module. The CTU module

* use one command list with 4 ADC_0 channels. Single conversion mode is used,

* so ADC0 ch0, ch1, ch2 and ch3 are sampled.

* ------------------------------------------------------------------------------

* Test HW:  MPC57xx

* Maskset:  1N65H

* Target :  internal_FLASH

* Fsys:     200 MHz PLL with 40 MHz crystal reference

*

* EVB connection:

*

* P8.1  - A[0]  .. GPIO output, used to see CTU-ADC ISR period

* P9.1     - B[7]  .. ADC0 AN[0] input

* P9.2     - B[8]  .. ADC0 AN[1] input

* P16.4 - I[3] .. CTU0 EXT TRG output

*

* see CTU0 EXT TRG output signal (toggle on each trigger) on P16.4 with respect of eTimer PWM signals.

*

********************************************************************************

GeneralRe: Example MPC5744P eTimer CTU ADC synchronization GHS614

Hi Pat,

Feel free to create a new thread. So others can also join a discussion.

If your questions are related to any issues in my examples than feel free to write here.

Peter

Tags (1)
No ratings
Version history
Last update:
‎11-19-2025 04:50 AM
Updated by: