1102212_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1102212_en-US

1102212_en-US

Tire Pressure Monitoring System (TPMS) - FXTH87

 

Demo Owner Mike Stanley

 

Tire Pressure Monitoring Systems (TPMS) help drivers with precise direct tire pressure measurement by providing individual tire readings – including the spare. NXP's world’s smallest, lowest-power, with highest memory for customer use TPMS is highly integrated with a pressure sensor, temperature sensor, accelerometer, MCU and a transmitter. Watch Mike Stanley explain the pressure sensor readings, temperature sensor display and the accelerometer/motion readings. These readings are time based periodic measurements where the data is given as an output to the driver.

 

Features

  • Simulation that portraits the TPMS as if it were inside the vehicles tires and sending reports to the vehicle's display unit about tire pressure
  • Module has the following: Pressure sensor, accelerometer, temperature sensor, low-frequency radio, Microcontroller

 


Featured NXP Products


Links

AutomotiveRe: Tire Pressure Monitoring System (TPMS) - FXTH87

How I can get Development kit or Reference design information of FXTH87 based TPMS? Thank you!

Re: Tire Pressure Monitoring System (TPMS) - FXTH87

I can not find the demo ,how Can I get it?

Tags (1)
No ratings
Version history
Last update:
‎12-09-2025 08:28 AM
Updated by: