1101580_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1101580_en-US

1101580_en-US

New Kinetis Expert Pins Tool V1.0 Available!

The new NXP Pins tool which has been showcased at FTF 2016 in Austin is now available as Web and Desktop application.

153130_153130.pngDesktop Version of Pins Tool.png

The Kinetis Expert Pins Tool makes configuring, muxing and routing of pins very easy and fast. It provides real-time feedback of conflicts and provides an intuitive graphical interface with several views. The tool generates Kinetis SDK V2.0 compatible sources files which can be directly integrated into C/C++ applications.

The Pins tool is available both as Web application (no installation needed) and as a Desktop application for Linux, Mac and Windows.

 

 

You can use the Web version from Welcome to Kinetis Expert | Kinetis Expert.

153199_153199.pngpastedImage_0.png

 

It is available for download as Desktop version from Software Development Kit for Kinetis MCUs|NXP

(Windows, Mac OS X and Linux 64bit) under the 'Software' category:

153268_153268.pngpastedImage_0.png

There are two different installer types:

  1. 'offline' is a 130 MByte download. This method is recommended for slower internet connections or for installation on multiple machines.
  2. 'online' is a small 500 KByte download, all the other installation data will be loaded from the internet during installation.

Mac OS X and Linux installers are 64bit. For Windows there are both 32bit and 64bit installers available.

 

Documenation is availble on Software Development Kit for Kinetis MCUs|NXP in the documenation download section, as well attached to this article (Getting Started is available in Chinese):

153204_153204.pngpastedImage_6.png

An overview and tutorial can be found here: https://mcuoneclipse.com/2016/06/08/tutorial-muxing-with-the-new-nxp-pins-tool/

 

We hope you find this tool useful!

GeneralRe: New Kinetis Expert Pins Tool V1.0 Available!

Hi Kevin,

Be aware that there is the V2 of the tools available now, see Kinetis Expert System Configuration Tools V2 with Clocks Tool now available! 

I quickly checked the downloads (I'm using FireFox), and that worked fine for me.

Software Development Kit for Kinetis MCUs|NXP 

Can you try again? I have seen reports that using Internet Explorer or Edge can cause issues or even corrupt the downloaded files.

I hope this helps,

Erich

Re: New Kinetis Expert Pins Tool V1.0 Available!

When I click to download I get a pop-up with the screen showing the ten items I could download but clicking on them has no effect. I double checked and I am logged in yet with the latest version of Google I can't download! I tried Microsofts Edge with the same results but it failed when I tried to edit this post... bad edge..

Re: New Kinetis Expert Pins Tool V1.0 Available!

That's great to hear! Being able to use the names in the sources will also be a welcome addition. This tool is proving to be very valuable.

Re: New Kinetis Expert Pins Tool V1.0 Available!

Hi Larry,

thanks for the suggestion. And yes, this is indeed something which is already considered and will be added to the next update/version: the ability to add custom label/names to each pin plus the ability to provide names which then can be used in the sources. The update is forseen to come out in the near future.

Re: New Kinetis Expert Pins Tool V1.0 Available!

Another nice-to-have would be to be able to override the pin names. For example, on a K64 I'm going to be using the FlexBus in a non-multiplexed 16bit address and data. It would be nice to be able to label them FB_ADDR0-15 and FB_DATA0-15, rather than the default of FB_AD0-31. Similarly being able to label gpio pins for their intended use would be helpful. When you are starting from scratch and trying to figure out what functions you are going to assign to which pin, meaningful (to the user) labeling simplifies the process.

Re: New Kinetis Expert Pins Tool V1.0 Available!

Hey Erich,

Glad to help.
Right now Kinetis development has so many moving parts.
I figured when I see something, blurt it out, and the tool developers may have a chance to include it in their next pass.

Thanks again,

  Steve

Re: New Kinetis Expert Pins Tool V1.0 Available!

Hi Steve,

many thanks for providing that feedback. I can reproduce what you report, and have reported this to the engineering team so hopefully they can address it soon.

Thanks again,

Erich

Re: New Kinetis Expert Pins Tool V1.0 Available!

Erich,

A couple more observations on the pin tool.
1) In Windows 7, or KDS, double clicking on an *.mex opens "Pin Tool v1.0".
    The problem is, it opens the last file used in the tool, not with the file selected.


2) In my project, I defined multiple function tabs: pmUart, pmSpi0, etc.
    After I saved it, I decided to re-order the tabs, which worked great visually.
    The problem was I couldn't save the order changes. The "save" was not available.
    Even "save as" didn't save the changes.

    Until I altered a pin attribute. Then I could save the tab changes.

Thanks again,

Steve

Re: New Kinetis Expert Pins Tool V1.0 Available!

Great! I saw your article, and then response here.
I Just tried it, and now the whole register is being updated as desired.

I was hoping there was a "trick". The tool seems fairly nice.
I'll play with the clocking next.

Thanks,

Steve

Re: New Kinetis Expert Pins Tool V1.0 Available!

Hi Steve,

this is controlled if the item is in italic font or not. See https://mcuoneclipse.com/2016/07/19/nxp-pins-tool-clock-gates-and-controlling-the-bits/

I hope this helps,

Erich

Re: New Kinetis Expert Pins Tool V1.0 Available!

Erich,

While using the pin tool (offline) I realized that the code generated only sets register values that are different from the expected hard reset values.
Based on the options being set, sometimes it generated the "short" version:

  PORT_SetPinMux(PORTA, PIN4_IDX, kPORT_MuxAsGpio);      /* PORTA4 (pin 38) is configured as PTA4 */

  PORTA->PCR[4] = ((PORTA->PCR[4] &

(~(PORT_PCR_PFE_MASK | PORT_PCR_ISF_MASK)))          /* Mask bits to zero which are setting */
  | PORT_PCR_PFE(PCR_PFE_ENABLED)                    /* Passive Filter Enable: Passive input filter is enabled on the corresponding pin, if the pin is configured as a digital input. Refer to the device data sheet for filter characteristics. */
);

Sometime the "long":

   const port_pin_config_t portb22_pin68_config = {

kPORT_PullUp,                                        /* Internal pull-up resistor is enabled */
kPORT_SlowSlewRate,                                  /* Slow slew rate is configured */
kPORT_PassiveFilterDisable,                          /* Passive filter is disabled */
kPORT_OpenDrainEnable,                               /* Open drain is enabled */
kPORT_LowDriveStrength,                              /* Low drive strength is configured */
kPORT_MuxAsGpio,                                     /* Pin is configured as PTB22 */
kPORT_UnlockRegister                                 /* Pin Control Register fields [15:0] are not locked */

   };

   PORT_SetPinConfig(PORTB, 22, &portb22_pin68_config); /* PORTB22 (pin 68) is configured as PTB22 */

For production systems, this is risky. A reset might not be coming from a POR restart, but a fault.
You would want to set the hardware to a definitive state, not assuming anything.

Is there an option that causes the tool to generate code the initialized all the whole register?
If not, I'll have to code the long method.

Thanks again for all your work,

  Steve

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-20-2025 01:17 AM
更新者: