1100830_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1100830_en-US

1100830_en-US

CAN FD and Partial Networking

Provide an overview of the protocol and implementation of CAN FD in system architectures, including the use of partial networking in relation to the deployment of CAN FD.

Provide an overview of the protocol and implementation of CAN FD in system architectures, including the use of partial networking in relation to the deployment of CAN FD.

Re: CAN FD and Partial Networking

I am using i.MXRTOS1170 EVKB. I am using sample project "evkbmimxrt1170_canfd_interrupt_transfer_cm7" but it is not working the way it should I am getting garbage data from transmitter. Any help. I configured CAN3 and LPUART1 no warnings or errors.

It is failing below 

mdkhaledibnhassan_0-1707219128390.png


Re: CAN FD and Partial Networking

If CAN FD communication is exposed to a CAN node, the CAN node willsee the CAN FD frame as an error and block the communication, thereby rendering the network useless. By using original CAN protocol on the CAN FD nodes all advantages of CAN FD are lost. prepaidgiftbalance

Tags (1)
No ratings
Version history
Last update:
‎11-20-2025 06:36 AM
Updated by: