Please ask questions about the RDDRONE-BMS772 board and software here
Hi @xete ,
It seems that the IC is powered and working.
A 4S battery (both LiPo or LiFePO4) is indeed in the correct supply range. That cannot be the issue.
Maybe a full disconnect (battery, programmer, serial interface) could help?
It could be a connection issue.
Can you try a slower programming speed?
Long wires and pin converters could impact the maximum programing speed.
You now use 1000kHz, "1000", can you try "100"? 100kHz programming speed?
If you would be able to upload a picture of the setup, that might show an issue.
Or provide the voltages on these programmer pins.
It would be interesting to know if the MCU is kept in reset or what VTref is.
Kind regards,
Cis
Hi @cisvmierlo ,
Thank you for the quick reply.
I was powering the BMS with a 4S battery. I was also using 3.3V TTL to USB to look at the serial output. The BMS was in the NORMAL state based on the LCD Screen and Serial.
It was connected to a J Link Compact Plus according to the pinout below.
Do let me know if you require any other info/suggestions for troubleshooting
xete_0-1768570899050.png
Hi @xete ,
Could you explain more about your setup in which you face an issue?
How did you power the RDDRONE-BMS772?
What is the status of the RGB LED on the RDDRONE-BMS772?
A picture of your setup would be helpful to be able to assist you in your problem with programming.
Kind regards,
Cis
I am trying to flash firmware on to the BMS.
However, I am facing this error when attempting to connect via SWD.
xete_0-1768568009515.png
Yes, we are currently testing the next release candidate of the open source BMS772 reference SW that includes DroneCAN support.
We would like to use the RDDRONE-BMS772 in our drone batteries.
My question is, if there already is a PX4 integration based on UAVCAN?
Is there any work which we can pick up?
Thanks in advance
Jan
After this voltage drop of the charger, will the charger stay off?
No at this point the charger will stay on. So it would restart the charge process if the current draw stopped. In the future we will implement a controllable charger to disable upon full charge.
Or will it have a lower voltage than your battery and the charger is protected against sinking the current?
No the charger is slightly higher in voltage to achieve full charge but it is also protected against reverse current.
Would it be feasible to increase the voltage level in which the BMS determines the charger has been disconnected? This way it may prevent the brown out of the computer. Then it would go back into charge state and protect itself from overcharging.
I will also intergrade a UPS as an alternative solution to the problem.
Thanks for your help
Hi All,
I am wondering is there anyway to read the type of fault code from the CLI? I can read the state (bms get state => FAULT) but is there a way to receive the type of fault e.g. over voltage?
If not do you have some guidance on the best way to implement that in the firmware?
Thanks for your help,
Lewis
Hi Lewis,
From reading your story I'm assuming the BMS is in the charge-complete state. With the power disabled to stop the battery from overcharging.
When your system draws more current than the still attached battery charger can provide, the voltage will drop.
In the charge-complete state, there will not be a current flowing from the battery, as the power switch is open. The BMS will check the output voltage too see if the charger is disconnected.
When the charger has this voltage drop and this drop is low enough for the BMS to think the charger is disconnected, it will go the SLEEP state, but it will first set the MCU in very low power run (VLPR) mode and other peripherals in lower power modes as well before closing the power switch.
After this voltage drop of the charger, will the charger stay off?
Or will it have a lower volage than your battery and the charger is protected against sinking the current?
Kind regards,
Cis van Mierlo
Thank you for your reply Cis van Mierlo, that was very helpful.
I was able to get the functionality I needed by using an N-Channel, P-Channel Mosfet with and RC timer to momentarily pull the wake pin low if a charger voltage is connected.
Another thing I am looking into is the time it takes for the BMS to wake from sleep state due to over current detection (i-sleep-oc). The issue I am facing that after a full charge the BMS output will be disabled to stop overcharging, if our robot then draws more current then the charger can supply the BMS will detect this and enable the output. However attaching the scope I have measured a switch time of the BMS of about 300-800ms. This delay is a problem as it causes a brown out for the raspberry pi.
I am wondering if there is a way to reduce this time? Maybe by updating the frequency it checks the output current to wake? If I can reduce the time I can the look into smoothing the voltage drop.
Thanks again for your help.
Lewis.
Hi Lewis,
Indeed, the BMS goes to deep sleep to preserve any charge left in the battery. Meaning that this will be the lowest power mode (±100uA).
The only way that this is feasible, is to turn off the VCC_3V3_SBC, which is used to power the MCU.
Meaning that the MCU will be off. So, setting an interrupt won't help with waking up from this mode.
The only to wake up from this is mode is to either re-apply a voltage to the BMS or to pull down the SBC's (U3) wake pin (pin 12).
Maybe use J22 to pull down the wake pin (keep in mind that the voltage on this connector is between the battery voltage and 0V). For example, you could use an external switch or signal controlled from your other system to pull this low.
Another solution would be to send the "bms reset" command over de CLI (UART) when you receive the undervoltage fault and the BMS is counting down before going into the deep sleep mode. This will reset the timer.
You could also reconfigure the timeout time for the BMS to go to deep sleep and even disable it.
To do this, see t-fault-timeout in chapter 8.2.2 (page 18) in https://github.com/NXPHoverGames/RDDRONE-BMS772/blob/main/BMS772_releaseNotes_5.0.pdf
Hopefully this will help, kind regards,
Cis van Mierlo
Hi All,
We are facing an issue with the integration of the NXP BMS into our ROV system and hoping for some guidance on the changes I should make to the firmware to resolve the issue.
The problem is we occasionally will deplete a battery during an ROV flight underwater, and the vehicle becomes unrecoverable as the BMS will go into deep sleep. Following an under voltage fault the BMS will enter deep sleep to reduce any further draw on the battery, part of this means turning off the UART communications. If we apply voltage to the BMS it will remain in deep sleep until the physical reset button is pushed. The issue is that the robot is deployed under the water, so physically pushing the button won't work and we aren't able to communicate via UART as it has gone into deep sleep.
So I am seeking any advice on how I might be able to overcome this problem. The goal would be to still have the BMS enter deep sleep mode to prevent further discharge of the battery however to be able to wake the battery via a UART command or if charge voltage is detected.
I was thinking I could attach an interrupt to the UART RX pin before entering deep sleep, which will reset the fault during wake up. Is this a feasible solution and if so is it possible for you to point me in the direction of the firmware I could do this?
Thank you for your help,
Lewis
Thank you that solution worked well for us.
Hi @lmiles-sosub,
The purpose of the gate check is to make sure the gate driver is able to turn off the power. It there would be something wrong with this or other components and it is not able to turn off the power, this could result in a safety issue, hence the self-test.
I get that for your purpose, this is not ideal. Feel free to disable this check in your software for your purpose if you think this is safe.
Keep in mind that it will not check if the power can be switched off.
Plus I would advise you to still turn off the power in that part of the code, you could either replace the part with the below piece of code or add compile switches (#ifdef #else #endif) so you could easily go back to the original state.
This part needs to be replaced or put in an compile switch: https://github.com/NXPHoverGames/RDDRONE-BMS772/blob/main/src/batManagement.c#L608-L672
This is the piece of code I would advice you to still add:
// still turn off the gate
batManagement_setGatePower(GATE_OPEN);
cli_printfWarning("SELF-TEST GATE: TURNED OFF!\n");
I hope this answers your question, kind regards,
Cis van Mierlo
Hi All,
We are testing the use of the BMS in an ROV system with a charger that constantly supplies power to the ROV and the battery will provide power for peak loads above the chargers power capacity.
We are having some issues when the battery reaches its under voltage protection (enters fault mode) and are trying to recover the BMS from fault state to be able to charge the battery.
Ideally the BMS would shut off output but would still allow a charge current to enter the battery, without needing to be reset. Currently we are resetting the BMS remotely through the CLI to remove the fault however to power the system we must have the charger on, which then results in the self test failing and suggesting to remove the charger.
My question is around the functionality of the charger having to be disconnected for the gate self test. What is the purpose of it and would there be a critical issue if I were to disable it in the firmware?
Thanks for your help.
Lewis
Hi @suvasis ,
The .brd layout file of the RDDRONE-BMS772 has been added to the design files and could be downloaded.
Please see https://www.nxp.com/design/designs/smart-battery-management-for-mobile-robotics:RDDRONE-BMS772
Kind regards,
Cis van Mierlo
Hi @cisvmierlo,
I tried rebooting and re powering the BMS it didn't help. I will try going into DEEP_SLEEP.
Thanks for your help.
Regards,
Prince
Hi @Prince1,
Have you tried rebooting the MCU with the "reboot" command?
Another thing you could try to reset the communication errors (as they are remembered) go to DEEP_SLEEP and back to NORMAL state?
Otherwise you could try to re-power the BMS power to solve the problem.
Kind regards,
Cis van Mierlo
Hi @suvasis,
I've asked the team if they could upload the board file (.brd) as well to nxp.com.
Be aware that this could take a couple days.
The schematic file (.DSN) is already included.
Kind regards,
Cis van Mierlo
Hi,
Tera term is throwing few errors when connected with BMS as shown in images attached herewith.
"Couldn't do measurements and also Failed to update measurements"
Please help in resolving them?
Thanks,
Prince
hi,
I am trying to redesign the PCB to a smaller form factor for my drone. The following document
https://www.nxp.com/design/designs/smart-battery-management-for-mobile-robotics:RDDRONE-BMS772
generally provides schematic and fabrication files but those link does not contain the source file of the PCB. can anyone include the source file for the PCB?
Can anyone help me?
thanks.
suvasis
Hi @dmorvay,
I think it would be possible to multiplex the I2CS to the PTA2/PTA3 pins.
I would check the S32K-RM chapter 52: Low Power Inter-Integrated Circuit (LPI2C) for this.
But then you need to make the correct changes in the code, I do not know if the SDK supports this.
Kind regards,
Cis van Mierlo
Hello @dmorvay,
Regarding the second question, the MBD Toolbox for S32K14x is built on top of the SDK for S32k14x. Unfortunately, it seems that the 4-wire mode is not supported for LPI2C by the SDK, therefore MBD toolbox doesn't support it either.
Best regards,
Bancila Sorin
Hi @cisvmierlo ,
Thank you for this information. I am still unsure about the answer to my first question - Can PTA2/PTA3 (J23) be configured as an I2C slave? Are there any limitations on this I/O that it always has to be configured as a master?
Hi @dmorvay,
I'm not familiar with the MBDT example and what is supported in that toolbox.
For a C / C++ example I would advise you to take a look into the NuttX RTOS SW example.
In this example you can get the BMS data via I2C by reading the correct I2C addresses as stated in Table 6. SMBus variable list (Of chapter 7.5 How to use SMBus).
This example is located here: https://github.com/NXPHoverGames/RDDRONE-BMS772
It will need the NuttX RTOS sources as well: https://github.com/apache/nuttx
See the RDDRONE-BMS772 board in the NuttX repository:
https://github.com/apache/nuttx/tree/master/boards/arm/s32k1xx/rddrone-bms772
And the S32K1xx architecture specific logic:
https://github.com/apache/nuttx/tree/master/arch/arm/src/s32k1xx
I hope this helps you!
Kind regards,
Cis van Mierlo
Hi @cisvmierlo
Two more questions based on your answer...
1. Can PTA2 and PTA3 (connector J23) be configured as an I2C slave? On the software side, it seems to be possible, but want to make sure everything checks out in both hardware and software.
2. How do you configure LPI2C0_SCLS and LPI2C0_SDAS? Do you have any references on how to configure this in C code and/or through Model Based Development? I am currently using Model Based Development, but I do not see any peripherals with LPI2C0_SCLS and LPI2C0_SDAS. Additionally, the I2C configuration block only has the options for PTA2/PTA3 or PTB6/PTB7. I am not exactly sure how to activate this output.
Hi @dmorvay ,
The connector J18 can be used for SMBUS / I2CS.
The SMBUS_SCL and SMBUS_SDA lines are connected to this connector.
These lines are connector to PTA0 and PTA1, which support the LPI2C0_SCLS and /LPI2C0_SDAS peripheral.
Kind regards,
Cis van Mierlo
Hi @cisvmierlo
Another question regarding I2C communication: when configuring the BMS772 as a slave, should the pins for SDA/SCL be PTB6 and PTB7 respectively or PTA2 and PTA3 respectively? Looking at the schematics, it seems like it is actually neither of these two options, but instead PTA0 and PTA1. Hence, I am slightly confused on how to setup the board as a slave for I2C communication.
Hello,
The PSMNR70-30YLH MOSFETS that are recommended by NXP documentation unfortunately are not available to buy in the sites I tried. This is an issue because I can not test with safety the board. I read in this community I can find it in Nexperia but the minimun quantity to order is 1500. I tried to look for another equivalent one but I cannot find it with the same characteristics. I don't know the tolerance or how much the MOSFET can differ.
The MOSFET characteristics recommended by NXP are below. What other characteristics are tolerated or what other suitable characteristics can you recommend, please?
N-channel 30 V
0.82 mΩ,
300 A logic level
MOSFET in LFPAK56 using NextPowerS3 technology
Thank you very much
Thank you so much @cisvmierlo . I think there was an issue with the reset signal. Now it's working, so thank you!
Hi @DaveNXP ,
Do you have access to an oscilloscope? And could you measure the if there are pulses on the MCU reset line?
Kind regards,
Cis van Mierlo
Thank you for your answer,
I already tried with the J2 connector(it is placed) thought JTAG lines, with the reset jumper and without it. And I still cannot connect to the target.
What could I do? How could I check the Reset line is properly connected and the signal is ok.
Thank you very much @cisvmierlo
Hi @DaveNXP ,
Could you check de reset line of the debugger? If it is correctly connected to the MCU?
Or if J2 is placed, maybe use this 2x5 connector to program the board via that programming header?
If J2 is not placed, maybe you could solder a 2x5 pin header in to program the board via that route.
Kind regards,
Cis van Mierlo
Does anybody know how to factory reset the RDDRONE BMS board(or awaken it)?
The board may be in deep sleep or in a state I cannot get it out.
At first I could connect to the core (Cortex-M4 identified) but after this, when I tried to flash the firmware, I cannot connect to the target anymore(log copied in previous post). So I cannot send any command with J-Link Commander. The voltage of the J-Link debugger is 3.3V. I pressed the physical button while board powered but nothing changed and it does not wake up.
This happened to the two RDDRONE boards I bought.
Please, any help would be really appreciated.
Thank you! @cisvmierlo @iaingalloway
Hi, thank you for your answer.
I tried pushing the SW1 button. I tried with the reset jumper and without it.
I tried generating a reset pulse with a signal generator following the electrical specifications in the s32k1xx datasheet. https://www.nxp.com/docs/en/data-sheet/S32K-DS.pdf
I checked all the voltages.
If I connect the FTDI cable some garbage slash noise appears in the Tera Term console when I turn on and off the switch power supply.
When you use JLINK software and a debugger to connect to the BMS, one of the first things JLINK.exe prints out is the voltage on the MCU/debug port.
It's possible that even with external power 22v or whatever, coming in to the BMS board, that the actual power supply feeding the MCU is not turned on.
There is a tiny physical button on the BMS which may wake up the MCU power supply.
https://nxp.gitbook.io/rddrone-bms772/user-guide/getting-to-know-the-hardware/board-organization
Hi Cis van Mierlo
The debugger provides 3,3V. And the output of the power supply connected to the RDDRONE board input is 22,2V. I do not understand very well what the problem may be and what changes and tests I should do.
I don't know any button to press or way to start it up again. I would really appreciate any help for this.
Thank you. Kind regards.
Hi @DaveNXP,
Could you check if the voltage is OK according to the debugger?
Maybe the SW put the system in deep sleep and a button press is needed to start it up again.
Kind regards,
Cis van Mierlo
Thanks for the answer cisvmierlo,
The thing is that at first I could correctly connect to the the core on the RDDRONE-BMS772 board, but after this first flash I cannot connect to core on the board anymore. So, I cannot send this 'h' command you recommend.
Do you have any other ideas?
Hi @DaveNXP ,
It seems that you can connect to the core, but not erase nor flash it.
Could you try to restart the J-Link commander and halt the core with the 'h' command?
Kind regards,
Cis van Mierlo
Hi,
I have a problem with the RDDRONE-BMS772 board.
I soldered the hardware "configuration pads" as recommended in the RDDRONE-BMS772 manual for a 6s battery.
Then, I connected the RDDRONE-BMS772 board to a 22.2V power supply for the first time, the onboard LED turned on.
I followed the steps in this guide from the "NXP Gitbook":
https://nxp.gitbook.io/nxpmobilerobotics/flashing-guide/flashing-hovergames-boards/windows
but after trying to flash the firmware bin file downloaded from the official github:
https://github.com/NXPHoverGames/RDDRONE-BMS772
with the recommended J-LINK debugger and I connected the cables as seen here:
The flash failed (log below), and I cannot connect to the RDDRONE-BMS772 board anymore. Furthermore, the LED does not turn on either. I am trying to re-flash it, but I cannot get J-Link commander to connect to the RDDRONE-BMS772 anymore.
If I try to access the board using an FTDI cable, I do not get any serial connection using Putty either.
I am a bit confused as I do not understand if the problem is that the CPU is halted, or the CPU is in a RESET loop, the CPU waiting for a RESET signal, the CPU is "locked" and I have to unlock it, or if it is something else.
Any help would be highly appreciated.
This is the log I got from the J-Link Commander console, in case it is helpful:
Type "connect" to establish a target connection, '?' for help
J-Link>connect
Please specify device / core.
Type '?' for selection dialog
Device>
Please specify target interface:
J) JTAG (Default)
S) SWD
T) cJTAG
TIF>s
Specify target interface speed [kHz].
Speed>1000
Device "S32K144" selected.
Connecting to target via SWD
InitTarget() start
SWD selected. Executing JTAG -> SWD switching sequence.
InitTarget() end - Took 55ms
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x24770011)
AP[1]: JTAG-AP (IDR: 0x001C0000)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Found Cortex-M4 r0p1, Little endian.
FPUnit: 6 code (BP) slots and 2 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7
[0][1]: E0001000 CID B105E00D PID 003BB002 DWT
[0][2]: E0002000 CID B105E00D PID 002BB003 FPB
[0][3]: E0000000 CID B105E00D PID 003BB001 ITM
[0][4]: E0040000 CID B105900D PID 000BB9A1 TPIU
Initializing 61440 bytes work RAM @ 0x1FFF8000
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
Memory zones:
Zone: "Default" Description: Default access mode
Cortex-M4 identified.
J-Link>erase
No address range specified, 'Erase Chip' will be executed
'erase': Performing implicit reset & halt of MCU.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
Erasing device...
****** Error: Failed to erase sectors.
J-Link: Flash download: Total time needed: 1.490s (Prepare: 0.603s, Compare: 0.000s, Erase: 0.885s, Program: 0.000s, Verify: 0.000s, Restore: 0.002s)
****** Error: Failed to restore target. RAMCode never stops
ERROR: Erase returned with error code -5.
J-Link>loadbin "C:\Documents\RDDRONE-BMS772-main\Binary\nuttx.bin" 0x0
'loadbin': Performing implicit reset & halt of MCU.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
Reset: SYSRESETREQ has confused core.
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Attach to CPU failed. Executing connect under reset.
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Could not find core in Coresight setup
Reset: Using fallback: VECTRESET.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.VECTRESET.
Reset: VECTRESET has confused core.
Reset: Using fallback: Reset pin.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via reset pin
Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).
Reset: Reconnecting and manually halting CPU.
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Attach to CPU failed. Executing connect under reset.
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Could not find core in Coresight setup
CPU could not be halted
Reset: Core did not halt after reset, trying to disable WDT.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via reset pin
Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).
Reset: Reconnecting and manually halting CPU.
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Attach to CPU failed. Executing connect under reset.
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Could not find core in Coresight setup
CPU could not be halted
Reset: Failed. Toggling reset pin and trying reset strategy again.
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Attach to CPU failed. Executing connect under reset.
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Could not find core in Coresight setup
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
Reset: SYSRESETREQ has confused core.
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Attach to CPU failed. Executing connect under reset.
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Could not find core in Coresight setup
Reset: Using fallback: VECTRESET.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.VECTRESET.
Reset: VECTRESET has confused core.
Reset: Using fallback: Reset pin.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via reset pin
Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).
Reset: Reconnecting and manually halting CPU.
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Attach to CPU failed. Executing connect under reset.
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Could not find core in Coresight setup
CPU could not be halted
Reset: Core did not halt after reset, trying to disable WDT.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via reset pin
Reset: VC_CORERESET did not halt CPU. (Debug logic also reset by reset pin?).
Reset: Reconnecting and manually halting CPU.
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Attach to CPU failed. Executing connect under reset.
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Skipped. Could not read CPUID register
Could not find core in Coresight setup
CPU could not be halted
CPU could not be halted
****** Error: Failed to halt CPU.
CPU could not be halted
Downloading file [C:\Documents\RDDRONE-BMS772-main\Binary\nuttx.bin]...
CPU could not be halted
****** Error: Failed to restore target. RAMCode never stops
Failed to erase sectors.
Unspecified error -1
J-Link>
Hi @dmorvay ,
The I2C voltage level is 3.3V.
This is the MCU voltage domain as well.
But there is 5V on the board which can be used to supply a display with 5V.
The schematic of the RDDRONE-BMS772 can be downloaded from the NXP webpage (click on design files or scroll down to the design resources):
https://www.nxp.com/design/designs/smart-battery-management-for-mobile-robotics:RDDRONE-BMS772
Kind regards,
Cis van Mierlo
Hi @cisvmierlo, I appreciate the information! I will try again on the display. For reference, what is the I2C transmission voltage on the BMS772? Is it 5V or 3.3V I2C? I don't want to hook up a 5V I2C (say Arduino) and then damage the board if it is 3.3V.
Hi @dmorvay,
Great that soldering the correct jumpers solves the cell voltage issue!
For the OLED display, as I said I'm not familiar with the Model Based Design Toolbox examples.
Maybe they mean the RGB-LED which is on the board with the LED example?
The display delivered with the kit should support 3.3V.
But if you are interested in an BMS example project written in C with the NuttX RTOS (this includes the display to showcase battery values), see the example here: https://github.com/NXPHoverGames/RDDRONE-BMS772
PS: This is a graphical display, not a textual display. So each character needs to be drawn according to a specific font that is used.
Kind regards,
Cis van Mierlo
@cisvmierlo That seemed to do the trick! It appears that I failed to read that portion of the documentation about soldering those jumpers.
Another question regarding the OLED screen, I tried building and flashing the LED example onto the board, but the screen would not turn on. Is there anything special I need to do there? I was reading 3.3V on J23 between VCC and GND, but when I plugged the screen in, it would not turn on. Any suggestions? I didn't get a chance to check the D34 and D35 diodes today, but do those need to be moved if I am reading 3.3V?
Hi @dmorvay,
I do not have experience with the Model-Based Development toolbox yet, so in this regard I can not check it.
For the HW:
Could you confirm that the soldered jumpers are SJ6, SJ10, SJ11 and SJ12 for 3S?
And the cell voltage filters are correctly in place:
cisvmierlo_0-1678950769358.png
Kind regards,
Cis van Mierlo
Hello, I was experimenting with the BMS772 this evening and was trying to display cell voltages. I have a 3s setup and for some reason one cell is consistently reading higher than the others. I confirmed via a multimeter that the cells are all roughly the same value. I tried this with two different battery packs as well. See my attached screenshot for more information. Notice, the BMS is consistently reading ~0.7 greater than the others. I am using Model-Based Development with a J-Link Debugger in FreeMaster. Any advice would be appreciated!
dmorvay_0-1678921034731.png
Hi,
Does BMS772 board support Pixhawk Cube Orange Autopilot?
I have successfully communicated with other UAVCAN devices such as Zubax ESC, Packet digital MPPT. links given below. But it didn't work with BMS772.
https://packetdigital.com/power-products/maximum-power-point-tracker/
https://files.zubax.com/products/com.zubax.telega/Zubax_Myxa_Datasheet.pdf
Also, Does BMS772 board support classical CAN (CAN 2.0) protocol? If yes, I would like to test it with Microchip's CAN bus analyzer.
Please clarify.
Thanks in advance..
This isn't helpful according to your question, but the code was developed using a segger jlink family device. If you are a student and this is non-commercial use, you can use one of the lower cost jlink-edu from suppliers like Adafruit.
The best reference for what is implemented is by referring to the actual code. Which is published and open source.
The Smart Battery System Specification ended up being helpful.
The spec sheet can be found here:
Request for Register Map for NXP RDDrone-BMS772
Hi all,
I recently purchased the NXP RDDrone-BMS772 battery management system for my project, and I am having trouble communicating with the device via I2C. I have been trying to read the registers of the device, but without a register map, it's difficult to know which registers to access.
I was wondering if someone could please provide me with a register map for the RDDrone-BMS772, or point me in the direction of where I could find one. I believe that having a register map would greatly help me to communicate with the device and extract the information that I need.
Thank you for your help in advance.
Best regards,
Hi @cisvmierlo,
Thanks for your help. I could solve Under voltage fault problem. Now I want to see DroneCAN / UAVCAN messages / parameters sent by BMS in some software tool.
Do you have some software GUI tool to see CAN messages from BMS?
I tried to see messages with DroneCAN GUI tool with BMS772 connected to Orange Cube Autopilot. But I am not successful. Mission planner software didn't recognize BMS in SLCAN mode.
Where as Cube orange detects other UAVCAN devices such as Zubax ESC, Packet digital MPPT.
Also, Should I change DroneCAN static node ID to other than 255 for it to work?
NXP's UCAN based nodes are not available for purchase in India.
Also, please clarify whether Over current, output short circuit protection is available on BMS?
Please clarify the above. Thanks again for your great support.
...
Hi @Prince1,
Great that the communication issue has been resolved!
For the other questions:
"Yes, CLI shows "Cell under voltage detected!" and display shows 11.26V although fluke instrument measures 11.7V."
The display shows v-out. Which is measured via a resistor divider on the output with 1% tolerance. Meaning that you could have a 0.946V difference on 26V, just because of the resistor tolerances.
So it could be that this is a little off with the actual value. In the current SW example there is no option to fine tune this measurement.
What you could do is: look at v-batt or add all the cell voltages together (which is the most precise). Vtot = v-cell1 + v-cell2 + ..
"1. It looks if cell voltages < 3.8V, it goes to Deep_Sleep. Will it happen even if load is connected on J5? I mean, if load is connected disconnecting the battery at 3.8V is too early when cell cutoff voltage is 3V."
So the default cell under voltage (for a LiPo battery) is set at 3V. You could check this setting via the UART interface via:
bms get v-cell-uv
You could set the cell under voltage you think is suitable with: "bms set v-cell-uv x.xV"
After setting parameters, do not forget to save it to flash with "bms save".
For more information on which parameters there are, please have a look at chapter 8.2 of BMS772_releaseNotes_5.0.pdf.
But I would check the cell voltages via the UART connection, so you can see which cell has a problem.
You can use: "bms get all" (gets all parameters), "bms show all 1" (updates the battery values), "bms show top 1" (updates the battery values without scrolling).
"2. Is it possible to reduce the voltage measurement error in BMS?"
As stated in the beginning, there is no parameter for correcting the v-out voltage.
But feel free to adjust the SW yourself so for example v-batt is displayed on the display instead of v-out.
Kind regards,
Cis van Mierlo
Hi @cisvmierlo ,
Thanks a lot.
You solved my problem.
After rectifying J19 connections, CLI and Display worked.
Yes, CLI shows "Cell undervoltage detected!" and display shows 11.26V although fluke instrument measures 11.7V.
1. It looks if cell voltages < 3.8V, it goes to Deep_Sleep. Will it happen even if load is connected on J5? I mean, if load is connected disconnecting the battery at 3.8V is too early when cell cutoff voltage is 3V.
2. Is it possible to reduce the voltage measurement error in BMS?
Kindly answer the above questions.
Thanks..
Hi @Prince1,
I think I found the issue with the communication on BMS1.
The black wire is connected to J19 pin 1, which is 3.3V and not connected to ground.
For ground, you need to connect the black wire to J19 pin 7 (other side of the connector).
Light blue is now connected to J19 pin 5 (SWD_CLK) and yellow is now connected to J19 pin 6 (RST_N).
I think you need to swap the connections on the connector J19.
I will come back on the other PCB later.
Kind regards,
Cis van Mierlo
Hi @CisvanMierlo,
I have attached images of two BMSes,
1st one: LED blinks in red for 1 min before going to Deep_Sleep.
2nd one: has over heat issue and LED doesn't turn ON.
Though I have used 5 pin cell terminal connector, I have not connected 4S pin (5th pin open) / wire. So, 5 pin connector is used for 3S battery. Voltages are correct at JP1 connector.
Today I charged battery to 11.7V and tested still same result.
Thanks..
Hi @Prince1,
Only with a cell under voltage detection it will go to deep-sleep after 1 min.
Maybe there is something with the cell connections.
could you perhaps share images of this board as well (top and bottom)?
Kind regards,
Cis van Mierlo
Hi Cis van Mierlo,
BMS default V-cell-UV may be 3V, but my all battery cell voltages are beyond 3.8V and 3S pack voltage is 11.5V. I think under voltage is not the reason for BMS going into Deep_Sleep.
Please mention what could be other reasons for BMS LED blinking in red for 1min and then going into Deep_Sleep.
D34 is placed, D35 not placed. Still Display doesn't turn on. Display pin numbers are connected as suggested.
I will share the images of other BMS board with over heating issue.
Thanks..
Hi @Prince1,
"BMS LED is blinking in red colour and then goes OFF after around 1min. I think it goes to SLEEP."
This indicates that there is a cell under-voltage detected (based on default battery technology: LiPo).
When this happens, the BMS goes to DEEP_SLEEP after t-fault-timeout (60s default) in order to preserve the battery with its lowest power mode.
In that DEEP_SLEEP state the MCU (and SBC) is turned off, so no communication is possible after that 1 min. The button is press (or a re-power) is the only thing to wake the BMS from the DEEP_SLEEP state.
So it could be that there is no communication because the BMS entered the DEEP_SLEEP.
Or there would be something with the connection.
For the display to turn on during initialization, could you maybe check that D34 is placed instead of D35?
For the other BMS setup, the SBC overheating and LED not turning on, indicates that there might be a short on the 3.3V domain (shorted to gnd).
Could you maybe show both of your boards (top and bottom side)?
Kind regards,
Cis van Mierlo
Hi GeraldP,
I have done the following on a new BMS,
SJ6, 10, 11, 12 are shorted for 3S configuration.
3S LiPo battery is connected to J4 and their cell balancing wires connected to JP1
pins 5, 4, 1 of FTDI USB UART are connected to pins 2, 3, 7 of J19 respectively and then connected to PC
115k2 8n1, Parity: None, Flow: None configured in COM port properties and Tera Term
The result is as follows,
BMS LED is blinking in red colour and then goes OFF after around 1min. I think it goes to SLEEP.
BMS output voltage at J5 is zero (load is not connected)
Tera Term window displays blank screen and doesn't take keyboard input
Display connected to J23 doesn't turn ON
Kindly help me in sorting out above issues.
I tried the same things on another BMS, in which LED doesn't turn ON and SBC chip is getting over heated.
Thanks..
Does anyone know where can I purchase other suitable debugger for NXP RDDRONE-BMS apart from J-Link or PEMicro ?? Thank you.
Hi GeraldP,
Thanks for your help. I will try the way you suggested.
Hi @Prince1, the SW will just report an error and power out will be not enabled if you have a battery connected that has different cell numbering than configured.
Battery needs to be connected to be able to configure the BMS.
So the way to setup the BMS is:
- connect your UART adapter and open terminal SW with 115k2 8n1 serial port setting.
- Connect balancer and main power connector of battery to the BMS
- see bootup sequence First start-up - RDDRONE-BMS772 (gitbook.io)
- configure the bms via command line Command Line Interface (CLI) - RDDRONE-BMS772 (gitbook.io)
bms set
- finish with bms save
if you type reboot the BMS will reboot with correct settings and will activate output in case no errors.
Hi,
I have PL2303HX USB To TTL(Serial) Converter which provides 3.3V on Tx, Rx and GND.
https://robu.in/product/pl2303-pl2303hx-usb-ttl-module-5-pin/
With this Can I attempt software reconfiguration?
PL2303HX will be inserted in USB port and its TX, RX, GND pins are connected to respective pins in J19 port. Do I need to connect battery also to BMS (to J4) to power it's circuit? If so, 4S or 3S battery?
As in my BMS, 4S cell terminal connector is soldered in JP1 and SJ3, SJ7, SJ11 and SJ12 are connected, but its factory default configuration in software is 3S. So, I am confused.
Thanks..
Hi @Prince1,
Yes you only need to connect GND, TX and RX as seen in this screenshot:
cisvmierlo_0-1674467103221.png
Keep in mind that a USB-TTL-3V3 is used, this ensures 3.3V logic level on the RX and TX pins.
Kind regards,
Cis van Mierlo
Hi iaingalloway,
Thanks for your reply.
I want to change the BMS configuration from default 3S to 4S and also change battery chemistry through serial console. Is FTDI type USB-UART cable connected to JST GH 7 pin connector (only Tx, Rx, GND pins) is sufficient for this?
I am also trying to get J link EDU mini debugger to update firmware, but it's lead time is 40 weeks. So, Just trying to update configuration parameters as of now.
Thanks..
I know this is now an old post, but I've cross posted and asked the model based design team to have a look here.
https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RDDRONE-BMS771-MBDT-question/m-p/158619...
Note also there has been some work done in NuttX/PX4 on CAN bootloaders. But these are incomplete at this time.
I wanted to note that there are also additional GPIO on the board that were allocated for this type of function to be added in the future as per a proposed DroneCode standard. There were some other potential for added features here, including identifying the battery to the vehicle etc.
In addition to code needing to be written,
These are located on a separate header and would need to be asserted on plugging in the battery to a drone or vehicle.
You will need to refer to the schematics on NXP.com for the details.
I am referring to the header J21 here:
iaingalloway_2-1674236410319.png
iaingalloway_3-1674236426257.png
Note that if you want to just use the serial console to see what is going on internally (and not reprogram and debug the board) Then you can buy any FTDI type USB-UART cable (or use a PC with a UART) to connect a serial console to the BMS772. Normally this is broken out on the DCD-LZ board so it can be plugged in easily.
Here is the type of cable you would buy at Amazon or Digikey or whereever:
https://www.digikey.com/en/products/detail/ftdi-future-technology-devices-international-ltd/TTL-234X...
iaingalloway_0-1674235896394.png
You would then use a JST-GH connector to attach to the RX TX and GND pins of the DCD-LZ interface on the BMS - do NOT connect the power from the FTDI cable to the DCD-LZ:
The pinout is shown here:
https://nxp.gitbook.io/hovergames/rddrone-fmuk66/connectors/debug-interface-dcd-lz/dcd-lz-breakout-b...
Thank you @cisvmierlo.
Very useful information.
iaingalloway_0-1673558852262.png
J2 is a socket for a standard 10/9 pin debug header that will work with any Segger JLINK device.
You can also make a cable to plug into the DCDLZ port and connect to a FTDI 3v3 USB2UART cable.
https://www.amazon.com/Pre-Crimped-Connectors-Pixhawk2-Pixracer-Silicone/dp/B07PBHN7TM/ref=sr_1_3?cr...
As noted, these items are included with some of the other development kits and can be re-used here.
Hi @Prince1,
Let me check internally about the availability of this adapter board.
Here is some more information about the DCD-LZ adapter board, including the schematic: https://nxp.gitbook.io/hovergames/rddrone-fmuk66/connectors/debug-interface-dcd-lz/dcd-lz-breakout-b...
I do know that they are usually part of a kit, I did find this UCAN board where you have the option to buy the KIT-UCANS32K1SIC.
This kit includes 2x DCD-LZ adapters, 2x FTDI-USB cable and 1x Segger Jlink mini EDU debugger (program and debug) as well.
Link to the KIT-UCANS32K1SIC: https://www.nxp.com/products/interfaces/can-transceivers/can-signal-improvement/can-sic-evaluation-b...
Kind regards,
Cis van Mierlo
In the following NXP community page it is stated that the documentation and software is available on DocStore. It also explains how to get access to DocStore.
So I believe the A1007 is available under NDA only.
Link to the NXP community page: https://community.nxp.com/t5/Other-NXP-Products/OM67201UL-driver-A1007/m-p/1447573
If you are looking to build something yourself, I would recommend to look at the common available NXP IoT Security and Authentication Portfolio: https://www.nxp.com/iotsecurity
For example, the SE050 or SE051 is a greatly supported device, with lots of use cases already implemented.
If you would like to develop on a board with an SE050 and a similar MCU (S32K146 instead of S32K144). The UCANS32K146 might be an interesting product.
Link to the SE050: https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-trust-se...
Link to the UCANS32K146: https://www.nxp.com/design/development-boards/automotive-development-platforms/s32k-mcu-platforms/s3...
I hope this answers your questions, kind regards,
Cis van Mierlo
A1007 Secure Authenticator
Hi community, I have just started developing with the BMS772. However, I can not find any information on the A1007 IC.
I can not even find this IC on the NXP site of any of our usual suppliers, Digi-Key etc.
Is this IC obsolete?
If so, are there any suggested alternative.
Thanks
Hi,
Thanks for your quick reply. Unfortunately, I couldn't find distributor to purchase DCD-LZ adapter in India. I don't have a hover games kit as well.
Can you suggest any alternative adapter which is widely available?
Thanks.
Hi @Prince1,
Indeed you would need to configure the software accordingly.
This can be done as followed:
1. Hook up the DCD-LZ adapter to the BMS772 board using the 7-pins JST-GH cable.
2. Hook up the DCD-LZ adapter to a laptop or PC with a FTDI USBUART-3V3 cable.
3. Connect to the BMS772 over a serial interface, like PuTTY or TeraTerm (115200 Baud).
4. Type "bms help" to get the help for the Command Line Interface (CLI).
5. Type "bms get all" to get all the parameters and the values associated with those parameters.
6. Change the variable you would like to change, in this case n-cells to 4, type: "bms set n-cells 4"
7. To make sure the parameters are saved to flash, type: "bms save"
8. After the new parameter settings, you could either press the button or type: "bms reset" to reset the fault.
The CLI is very useful as it will indicate what caused the error.
Here are some useful links to get started:
A link about setting up the CLI: https://nxp.gitbook.io/rddrone-bms772/user-guide/getting-started-with-the-rddrone-bms772/using-the-c...
A link about using the CLI: https://nxp.gitbook.io/rddrone-bms772/software-guide-nuttx/command-line-interface-cli
A link with a list of parameters: https://nxp.gitbook.io/rddrone-bms772/software-guide-nuttx/untitled-1
Chapter 7 of the release notes (rev. 5) is useful as well as this contains a picture of the DCD-LZ adapter with the 7-pins JST GH cable and the USB-TTL-3V3 cable connected to it.
Chapter 8 includes the parameters of the BMS772.
I would recommend the update the software to the latest binary.
The latest binary can be found at: https://github.com/NXPHoverGames/RDDRONE-BMS772/tree/main/Binary
Instructions can be found in chapter 7 of the release notes, on the code repository or on the gitbook: https://nxp.gitbook.io/rddrone-bms772/user-guide/getting-started-with-the-rddrone-bms772/flashing-fi...
Keep in mind that after programming, you need to re-configure the parameters again as these get overwritten.
I hope this helps, kind regards,
Cis van Mierlo
Hi,
I bought a new RDDRONE-BMS772 board and want to use it for 4S LiPo battery pack. I have soldered Cell terminal connector and Solder jumper pins (SJ) for 4S. After connecting to 4S pack, When I measured the output voltage it is 0V. I don't know why.
Shall I do any configuration change(for 4S) in the software also? If so, how? Please reply.
Thanks in advance.
Hi @Ch_Han,
When the BMS is in the DEEP_SLEEP state it needs to limit the power the BMS is using itself, in order to preserve the battery the most.
This is done by setting the components powered by the battery in a deepsleep / sleep state as well and by disabling the voltage domains (3.3V and 5V are turned off), amongst others, powering off the microcontroller, which is supplied by this 3.3V.
To initiate a wake for the SBC (to turn on the 3.3V again which will power the microcontroller), I believe the SW has only configured that the wake pin of the SBC, issues an SBC wake. To do that, the button needs to be pressed or J22 needs to be shorted.
But I do believe a wake-up via CAN could be enabled in the SW, as the SBC is in a sleep state and still powered by the battery. This is however not enabled by the current SW example and I do not know the HW requirements for this.
If you would like to add this functionality, you could check the datasheet of the SBC and the sbc.c and sbc.h files of the public BMS SW example for this board.
The datasheet of the SBC can be found here: https://www.nxp.com/products/power-management/pmics-and-sbcs/mini-sbcs/mini-high-speed-can-system-ba...
Kind regards,
cisvmierlo
Thank you for your answer.
Then if the battery is in storage with the BMS in DEEPSLEEP state, can the BMS detect when the output is connected to go back to NORMAL or is the only way out of DEEPSLEEP by pushing the button?
Regards,
Hi @OGUZ1,
I wanted to let you know that the RDDRONE-BMS772 board is now supported in the NXP Model-Based Design Toolbox (MBDT) for S32K1xx - version 4.3.0.
Here is the Product Release Announcement: https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/NXP-Model-Based-Design-Toolbox-for-S32K1xx...
The NXP MBDT includes an integrated Simulink®-embedded target supporting NXP MCUs for direct rapid prototyping and built-in support for software- and processor-in-the-loop (SIL and PIL) development. https://www.nxp.com/design/automotive-software-and-tools/model-based-design-toolbox-mbdt:MBDT
Kind regards!
Hi @Ch_Han,
Please see https://github.com/NXPHoverGames/RDDRONE-BMS772/ for the release notes. This describes the state machine of the BMS example software.
The SLEEP state is not for storage, as in this example the output power is still enabled in this SLEEP state. For storage, the BMS should indeed go to the DEEPSLEEP state, where the output power is disabled (power switch is open) and the current is as little as possible.
In chapter 8 of the release notes, the parameters are described to control the BMS. If you set parameter self-discharge-enable to 0. You could go to the DEEPSLEEP state without discharging the battery cells to storage voltage. Keep in mind that this might not be good for the battery cells if they are at a high voltage for a long time.
In the self-discharge state, the BMS will use the balancing current to discharge all the cells to be less than the set storage voltage (with margin).
In SLEEP state, the switch is always closed in this example, enabling the output power. Thus, it could detect a load by measuring current.
I usually work with a lab power supply to charge the batteries.
PS: You could develop your own software or adapt the SW for your needs based on the open source example on https://github.com/NXPHoverGames/RDDRONE-BMS772/.
Hopefully this answers your questions, kind regards,
cisvmierlo
Hello @iaingalloway @cisvmierlo ,
I plan to use the BMS772 with 6s LiPo batteries, and have questions concerning the charge and discharge.
1- Is there a way to store the batteries without discharging? I see that before going into DEEPSLEEP state where the gates are open, the BMS must go through a SELF-DISCHARGE state; or if the BMS is in SLEEP state the gates are closed which also leads to discharging.
2- What is the physical process of the self-discharge?
3- Has measuring the impedance through CAN been thought of to detect if an output is connected? For example to know if gates should be open or closed in SLEEP state.
4- Is there a recommended charger to charge the batteries with a limited current? Or at least which one do you use usually?
Thank you.
Hi @vikrantj,
Since you are doing this for a school project, I think you are able to buy a J-Link EDU (mini).
This is a cheaper version of the normal J-Link meant for educational purposes.
Here is a guide on how to use the J-Link EDU (mini) to flash the RDDRONE-BMS772: https://nxp.gitbook.io/nxpmobilerobotics/flashing-guide/flashing-hovergames-boards.
Would this help you?
Kind regards,
Cis van Mierlo
Hello @vikrantj,
I did not have the chance to use this board yet. But having a look at the schematic, the easiest way to flash this board directly from Simulink without using a JTAG all the time is to use the RAppID bootloader, over the UART. Of course, you have to flash the bootloader once using a JTAG but once you have the bootloader written in the flash memory, you can use the Serial, directly from Simulink.
You can find a suitable bootloader in the toolbox, under tools\BootLoader\RBF_Files the S32K144_S32DS_UART1_CAN0.rbf which uses the pins PTC6 and PTC7 over the DCD-LZ. And here, you can use an external USB2Serial converter.
Also, the CAN0 can be used to deploy the code on the board, but you need to use the RAppID bootloader app, and a compatible CAN tool.
Let me know if Serial is a good option for you.
Regards,
Marius
Hello,
I am using the RDDRONE-BMS772 to build a 3s li-ion cell cycler. I wanted to be able to flash the program to the S32K on the board using a CAN bus. I was wondering if there is any way to do this. Or is using a debugger the only way to flash the program? If there are any other alternatives you could suggest I would appreciate it. This is for a school project and hence I need to keep the costs (and the complexity) low.
@OGUZ1 , @iaingalloway, @mariuslucianand I would love to know your thoughts about this.
Hi, @cisvmierlo
Thank you very much for your reply.
Yes, I'm using SPI0 but I can't see any effect. I always read something like 2.7Volt from pin V2. I always read 3.3 volts from V1 pin. I still read the same values when I press the reset button. I couldn't figure out what it means. I tried all the configurations. Vbat and Wake pins are the same value in SBC.
When I press reset, the Wake pin drops to 0. 3.3 volts is always going to the SBCWake pin of the processor.
Hi @OGUZ1,
Sorry I do not have experience using MBDT in Matlab / Simulink.
For the help with the model based design toolbox and SBC 5V problems. @mariuslucianand could you help @OGUZ1 further with this?
It could be that the UJA1169 configuration might be meant only for the S32K144 evb board, which could be different than what should be used on the RDDRONE-BMS772.
For example, on the S32k144 evb LPSPI1 is used to communicate with the SBC.
While on the RDDRONE-BMS772 LPSPI0 is used.
Could you verify that the correct SPI bus 0 is used to communicate with the SBC?
According to @constantinrazva the SBC driver is located in the external devices.
Could you verify that you are using this SBC block?
If you are interested to see how to set the SBC using C code, here is an example: https://github.com/NXPHoverGames/RDDRONE-BMS772/blob/main/src/sbc.c
This enables the 5V in normal operation of the SBC.
For the display, we have example code how to use the display with the NuttX RTOS.
See https://github.com/NXPHoverGames/RDDRONE-BMS772/blob/main/src/display.c.
It uses the characters and drivers from this NuttX RTOS.
The display itself is a SSD1306 I2C display that works at both 5V and 3.3V.
I believe there are many C examples of how to work with this kind of display.
For example: https://github.com/adafruit/Adafruit_SSD1306
For MATLAB maybe these sources would be able to help as well: https://nl.mathworks.com/matlabcentral/fileexchange/50766-ssd1306-hex-bitmap-creator?s_tid=srchtitle or https://nl.mathworks.com/matlabcentral/answers/512483-how-to-control-ssd1306-128x32-oled-display-in-...
Kind regards and have a nice weekend,
Cis van Mierlo
I want to run the screen via Matlab/Simulink. Can you share any example with me? I can see the battery values with Matlab/Simulink. I want to use CAN communication but I still can't get 5V from SBC. I still could not get 5V output from SBC. Are you interested in me?
Best Regards!
Hi @OGUZ1,
Please see https://github.com/NXPHoverGames/RDDRONE-BMS772/ for the NuttX RDDRONE-BMS772 BMS example. Documentation, source code, binary and a manual can all be found at that website. It uses the POSIX compliant RTOS NuttX. That example contains the things like SSD1306 display support and configured SBC for 5V.
If Matlab/Simulink, FREEMASTER or something else is used to re-program the boards, there might be different software running on the microcontroller and thus it won't have the correct behavior and functions. You are free to re-program this board/microcontroller with the software you want (or make!), but make sure that what you program is what you are looking for.
If you would like to create your software, you could create it based on sources from https://github.com/NXPHoverGames/RDDRONE-BMS772/. This could help you get started with NXP components like the SBC (UJA1169), the BCC (MC33772B) or the NTAG5 boost NFC chip. If you want to program the NuttX BMS example, there is already a binary on that website/repository which you could easily program using the J-Link commander application (for windows (or JLinkExe on Linux)) and a J-Link programmer.
Hi , @iaingalloway @cisvmierlo
I programmed the RDDRONE - BMS772 board with Matlab/Simulink. I see all values in FreeMaster.
I have a few questions...
1) I want to run the SSD1306 screen on the card. I changed the D34 and D35 diodes. 3.3Volt appears on the screen, but it does not work. Could you help ?
2) We give 1 to the Gate leg of the power mosfets of the card from the software and we get the output voltage. Why do we still get output voltage when we give logic 0 from the software? (We tested it with the load connected.)
3)Although we operate the SBC in normal mode, we cannot get 5V output. We only get 3V3. We are using sbc_uja1169_s32k_config. Although we activate the V2/VEXT config section in the regulator section, we cannot get output from V2. What is the reason of this? Can you help us?
Hi @Prince1,
First of all, best wishes for this new year!
My apologies for the late response, we had some time off.
To answer your questions:
The BMS772 comes with pre-installed example software, but you might want to update it to the latest version. But keep in mind that it is a development platform with open source example software. This software is opensource and provided for development purposes and not warranted for end use. You will still need to ensure that the hardware and software meets your needs.
Currently we have not tested the BMS with multiple packs in parallel. It could be that the hardware could accommodate it, but the software and state machine would need to be reviewed for correct operation in parallel configuration.
There is a self-test build in which will test if the MOSFET can be switched off during startup. This to ensure the MOSFET and its control circuitry is fully functional and can be used for HW/SW OC/OV/temp protections (see SW release documentation). What happens to the batteries depend on the scenario, is it charging or discharging, does it need to connect or disconnect the batteries using the MOSFET. Plus the BMS is not the same as a battery charger. An externally controlled constant current (CC) constant voltage (CV) source is still required to charge the batteries.
Currently the BMS has on-board balance resistors plus FETs inside the installed BCC chip to balance the cells, a command from the MCU to the BCC enables or disables balancing for each individual cell.
I hope this answers your questions!
Hi,
We want to use RDDRONE-BMS772 for solar drone with 20 Nos. of 4S battery packs in parallel. Please clarify the following queries,
1. Can RDDRONE-BMS772 board be used readily or any software to be uploaded before using?
2. Can we connect 20 nos. of BMS772 in parallel to charge 20 no. battery packs (each pack has 4S cells)? If yes, any additional protection to be provided externally?
3. Is there any inbuilt protection to prevent MOSFET failure in BMS772? If not, what happens to batteries when MOSFET fails?
4. Are external MOSFETs required for Active cell balancing? How active cell balance works in BMS772?
Thanks in advance.
Hi @coryjfowler
We're actively investigating the issue. We needed to get some of the current build of boards from the warehouse in order to determine what is going on with this latest board build. A workaround will be provided shortly while we determine the root cause. Thank you for your patience.
@cisvmierlo
Can I get some help with my V 4.0 REV D board and the issue with the NFC chip that causes a full stop of the BMS application? Last reply to the Github issue was 3 days ago. I was anticipating a reply this morning, but no such luck.
Hi KarenRdz!
Yes that is possible.
J19 combines the JTAG debugger pins together with the UART pins, the UART pins are needed for the CLI.
There is a DCD-LZ breakout board which lets you connect your JTAG debugger to the JTAG debugger pins (like J2) of that breakout board and separates the UART to FTDI pinout.
This could be connected to J19 of the BMS.
See https://nxp.gitbook.io/hovergames/rddrone-fmuk66/connectors/debug-interface-dcd-lz/dcd-lz-breakout-b... for more detail on the breakout board.
Connector J2 is only a 10 pins JTAG connector, without UART pins.
You could use J2 to program/debug the board and use J19 for the CLI.
As an alternative to that, connector J21 has another UART bus on it.
Since the code is publicly available and it uses the NuttX RTOS, it could easily be changed in using the other UART bus for the CLI.
You could select LPUART0 as serial console in the menuconfig of NuttX (in Device Drivers -> Serial Driver Support -> Serial console).
So then you could use J2 for programming/debugging and J21 for the CLI if you configure it.
Hi!
I have a question, is it posible to use the CLI if the J-link debugger is on the J2 port? Or is there another way to obtain the information on the J2 whitout using the CLI?
Thank you!
Yes - sorry to hear that. I also looked, and you are correct, there doesn't seem to be global availability. This is an active and good part, it is just caught up in the global chip shortage.
Here are some (not so great) options:
- Contact Nexperia directly. You only need a few correct? Sometimes there are samples they have on hand.
- Look through Nexperia.com for close alternatives?
- Buy an additional BMS-772 and take the parts off one to add to the other?
Due to the chip shortage the PSMNR70-30YLH mosfet is no more available in the market. What to do with that, is there any other mosfet we can use with that model. Please reply me soon as we need this product as soon as possible.
Hi Anuj,
The FRDM33772BSPIEVB is an evaluation board for the battery cell controller. This is without microcontroller, switches, safety measures and etc.
The RDDRONE-BMS772 is a mobile robotics reference design including microcontroller, power switch, (working and available) example software, hardware overcurrent circuit and more.
For more information about the RDDRONE-BMS772 see: https://nxp.gitbook.io/rddrone-bms772/
For the example software see: https://github.com/NXPHoverGames/RDDRONE-BMS772
The RDDRONE-BMS772 as populated is rated for 60A continues DC current.
With 4 pairs of MOSFETs and 4 heatsinks it is rated at 90A maximum DC current (continues) and this includes the layout and copper used.
On the RDDRONE-BMS772 there is a hardware overcurrent circuit at 545A which will act within 20us.
Which means a peak current of 545A is allowed for 20us without damaging the board.
Higher currents or currents for a longer amount of time might be possible, but has not been tested.
Going over the maximum rated currents or the specified time will be of own risk.
Keep in mind batteries should always be handled with care.
We are working with solar drone which requires a lot of power.
This product seems very nice but i am confused on the maximum rating. We have 6s configuration Lipo battery which is 22 volt, and the motor can require a huge burst current and continuous current(90A for minutes). I see that the maximum rating for this is 90A DC, Is this value continuous maximum rating or burst maximum rating. What is the burst current and time limit for the burst current. Can you please suggest me which can be better for me this one or the other BMS FRDM33772BSPIEVB.
Hope i get a very fast reply.
The BMS772 does the self balancing. You will need to control the overall current provided to charge the battery. You should also provide some power steering/isolation otherwise with the two batteries in parallel, the higher charged one will attempt to charge the lower charged one.
Also - what is not clear above - are you making one pack or two separate pluggable packs. You CAN parallel individual cells in one large one (and use a single BMS) if you wish, but that does not seem to be how you have described it. So one BMS per pack is needed.
The BMS is approximately the size of a 3S 4000mA/h hobby LiPo - Sorry i do not have exact dimensions.
Thanks for the update and quick reply. I'll be sure to keep an eye on this thread. Looking for the same issue. Bumped into your thread.
Hi there,
we have a drone battery that consists of 2 x 7000mAh 6S lithium polymer batteries. These two packs are going to be connected in parallel to achieve 14000mAh 6S.
What I did is made a housing to incubate the two packs and connected them to a single 10 pin robust male connector and in the UAV size there is a female connector . The plan is to make the drone battery like cartridge so we can slide it in UAV to click in and go on and when battery need recharging we take out the cartridge and connect it to the charger with same pin type used on UAV. The question is are we able to use you BMS 772 to achieve a self balancing cartridge when recharging?
if so how would we do that? Do we need two boards or one only? And how to connect it to the batteries?
and what’s the dimensions of that board please?
best regards
Falcon
Hello @SH ,
This depends on what you would like to test.
If you would like to have voltages on cell measurement tabs. Without charging or (passively) balancing the cells. You can easily add some resistors over your voltage supply to mimic the cell voltages and measure them with the BMS772.
For example you have a lab power supply and you would like to test a 3S battery (3 cells in series) setup.
You can set the lab power supply to 12V attach them to the power in + and power in - of the BMS. Parallel to that you add a voltage divider with 3 resistors of for example 1kΩ in series from power + to power -.
You can add the 4 balance wires to these resistor (+, - and the 2 in between resistors) to connect to the balance lead connector JP1.
Make sure to solder the BMS for 3S configuration according to the release notes on github: RDDRONE-BMS772/BMS772_releaseNotes_6.0.pdf at main · NXP-Robotics/RDDRONE-BMS772 · GitHub
I would suggest to download this release note PDF as the viewer is clipping the document.
There should be ~4V per "cell" in this setup.
You should be able to start up the BMS772 in normal mode when you power on the lab power supply (current limit could be set to 100mA without a load).
As long as the BMS and power supply is able to handle it and configured for it, you can add a load to the output of the BMS772 as well.
I hope this helps!
Kind regards,
Cis
Hello,
I am using the BMS-772 for a university project and do not have access to the battery cell emulator. I was wondering how design a resistor setup on breadboard to mimic the battery cells for purely testing purposes temporarily.
Thank you for any help,
Shane.
HI @cisvmierlo ,
Thank you for your help. Lowering the clock speed solved the issue.
Hello again,
Thank you for your help. I have a second BMS-772 board and have soldered the 3 cell connector to the board and I am using a three cell configuration with resistors mimicking cells. However, the CLI always gives me 0v for the 3rd cell and therefore an undervoltage error. There is voltage across the 3rd resistor. I got some solder across the cell setup pads on the bottom of the board but removed most of it. What could be the issue here?
Thank you again for any help,
Shane
20260404_171220.jpg
20260404_171231.jpg
20260404_171422.jpg
Hi @Shane93 ,
Thank you for reaching out for a question on the RDDRONE-BMS772.
And thank for sharing the helpful images!
Would it be possible to verify the solder connections to make sure the BMS is configured for 3S?
From the image it looks like SJ2 is connected, while SJ12 and SJ10 might not be connected?
If you have a multimeter with resistance measurement, you are able to check with (with resistors removed and the board not powered).
Here you can find more information on the solder jumpers for the cell configuration (3S): https://nxp.gitbook.io/rddrone-bms772/board-user-guide/getting-started-with-the-rddrone-bms772/confi...
Another thing that I notice is that you are using a bread board and Dupont jumper wires. Keep in mind that these are known to have bad connections. I do understand that for debugging this might be easy to do. But a bad connection because of the breadboard and / or the wires could also be a problem.
From what I can see in the image, the way you connect it is OK.
I'm also curious about your settings.
If you type in the CLI / UART command window the following command:
bms get all
What do you see?
I would like to see the n-cells you have configured for example as default this is 6 cells.
You can find which commands to look at in the Chapter 6 Getting started / quick start guide of the release notes (page 9 of 59): RDDRONE-BMS772/BMS772_releaseNotes_6.0.pdf at main · NXP-Robotics/RDDRONE-BMS772 · GitHub
Chapter 6.4.1: The most important BMS variables lets you know what to configure when you start with a BMS. Like n-cells.
You can change n-cells to 3 (in your case) with the command:
bms set n-cells 3
That should make sure the BMS doesn't check the other 3 cells that are not present in your setup.
I hope this helps!
Kind regards,
Cis van Mierlo
Hi @cisvmierlo
Thank you for all your help. The solder pads seem to be connected, when I run a "bms get all" I get this return. However, measuring across the 3 resistors gives me the natural step down of 12v, 8v, 4v, 0v.
Thank you,
Shane
image_2026-04-08_115330382.png
Thank you very much for you help. Two of the surface mount resistors had lifted on the back of the board causing an error in the cell reading circuit. The issue is resolved now thank you again. I have one final question you might be able to assist with. I am building my own custom CAN interface using NI-XNET with Cyphal CAN. Can you tell me how the CAN frames are structured and the addresses? Also is it possible to turn off the output voltage by controlling the MOSFET's over CAN?
Thank you,
Shane
Hi @Shane93,
Good that you have found this issue with 2 SMD resistors and thank you for sharing this information.
I believe both CyphalCAN and DroneCAN information can be found in the release notes.
It will mention which messages are implemented.
There is no direct message in either protocol that can turn off the power switch.
With DroneCAN, you can easily change settings and might be able to create an error in which the BMS will turn off the power. For example, changing the overtemperature setting.
You should be able to change the setting back to a "good" value and reset the fault.
This has been tested with DroneCAN.
But if you are creating your own custom CAN interface, you can add this feature yourself.
I hope this helps.
Best regards,
Cis