1071160_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1071160_en-US

1071160_en-US

MPXV5010 Accuracy over a Reduced Temperature Range

Hello,

The datasheet for the MPXV5010 pressure sensor only states the accuracy over a temperature range of 0-85oC. Can you provide any data about the accuracy of the MPXV5010 pressure sensor over a narrower temperature range? Preferably 15-40oC?

Thank you for your help.

Pressure SensorsRe: MPXV5010 Accuracy over a Reduced Temperature Range

Hi,

MPXV5010 is temperature compensated on the range from 0 to 85oC, the amount of error (accuracy) caused on this complete range is the same. Check the “Temperature Error Band” image on page 6 of the datasheet (https://www.nxp.com/docs/en/data-sheet/MPX5010.pdf), here you can find that the error multiplier on the complete operational temperature range, and for the range from 0 to 85 is the same as 15-40oC (multiplier of 1).

Regards,

Jose

NXP Semiconductors

Tags (1)
No ratings
Version history
Last update:
‎02-04-2026 08:33 AM
Updated by: