searching example for pwm generation for B-6 inverter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

searching example for pwm generation for B-6 inverter

763件の閲覧回数
AnweshaPanda
NXP Employee
NXP Employee

Hello, 

Is there any example code in i.MXRT series 1050/1060/1160/1170 etc. uCs that generates 6 pwm signals to stage test the status of the B-6 inverter. Although the end use is for motor control, I am not looking for an entire motor control solution example here. 

0 件の賞賛
返信
1 返信

739件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

With RT series it is possible to generate PWM signals with different timers (FlexIO, TMR and eFlexPWM). For motor control eFlexPWM is your best option.

There are SDK examples, but not the one that require.

I consider that the best way to follow is to refer to the PWM configuration from motor control demos in MCUXPRESSO-SDK-MOTOR-CONTROL.

On the other hand, there is the app note AN14196 Flex Pulse Width Modulator (FlexPWM) Usage on MCX N Series, with its respective associated SW file (AN14196SW). This is for another MCU but it uses the same module and its configuration should be quite similar.

Hope it helps you.

Have a nice day!

0 件の賞賛
返信