example NXP S32K Position FOC control mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

example NXP S32K Position FOC control mode

3,162 Views
michelet1
Contributor II

hello,

i would need to add position FOC control mode to a motor control example for s32k1.

I wanted to take hint from an existing example but i didn't find any NXP examples for motor control s32k that implemented position control. Do you know if there are any examples to start from?

Thanks in advance

 

3 Replies

3,144 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

All the examples available about S32K1 you can find in MCSPTE1AK144.

Hope it helps you.

Have a nice day!

0 Kudos
Reply

3,125 Views
michelet1
Contributor II

Hi,

thank you for your reply.

Right now i'm already using the project MCSPTE1AK144.

However, this project does not include position FOC control.

Are there other motor control projects of the s32k(k1,k3 ect...) which include position foc?

just to take a cue from a position control already created also to see which functions of the Automotive math and Motor Control library(MLIB,AMCLIB etc...) it uses to create position control.

Any point to understand how to implement a position control within the project MCSPTE1AK144 would be very useful and interesting for me.

Thanks again for your help.

0 Kudos
Reply

3,111 Views
_Leo_
NXP TechSupport
NXP TechSupport

The examples of the MCSPTE1AK344 are also available, but they also do not include the position FOC control.

Sorry for the inconvenience.

0 Kudos
Reply