current controller calculations MCAT tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

current controller calculations MCAT tool

1,871件の閲覧回数
WimvanderSteeg
Contributor I

I'm using the MCAT tool for developing a new BLDC based motor control application (E-Boat). This tool is used to get the motor running in a basic configuration. Attached in the zip file, you will find screenshots of the tool, with values as used for the motor. When switching to the current controller tab, 2 errors do pop up (see attached zip file with screenshots). Has this to do with the used motor type (high voltage - high current)? Is there a document available how the values for the current controller are calculated form the motor parameters? (to check where the calculation goes wrong, it is expected that some values gets too small or too big somewhere in the middle of the calculations.

タグ(2)
0 件の賞賛
返信
1 返信

1,712件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check the application note AN4870 , the chapter 5 MCAT tool for BLDC motors provides parameters introduction.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信