Using NXP for Controlling 3 phase Induction Motor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using NXP for Controlling 3 phase Induction Motor

Jump to solution
2,395 Views
ahmed_kamal
Contributor I

Hello everyone, I intend to build a new 3 phase AC induction motor drive using one of NXP Devkits. I will use sensorless field oriented control technique. Until now, i am thinking to use NXP MPC5744P Devkit but I need your help if is that a good choice or not? Also i need to find an example SIMULINK model to help me.

1 Solution
2,379 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, you can use MPC5744P. There are also new micro based on ARM core which are more suitable for motor control but MPC5744P is just fine.

If you like have a look at S32K1 / S32K39x for basic or more advance devices. AMMCLIB for simulink is available.

https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-auto-gener...

Best regards,

Peter

View solution in original post

1 Reply
2,380 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, you can use MPC5744P. There are also new micro based on ARM core which are more suitable for motor control but MPC5744P is just fine.

If you like have a look at S32K1 / S32K39x for basic or more advance devices. AMMCLIB for simulink is available.

https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-auto-gener...

Best regards,

Peter