Project Examples for HVP-MC35HP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Project Examples for HVP-MC35HP

3,226件の閲覧回数
harsh_kumbhar
Contributor I

I am working on PMSM motor Drive. For this we are using HVP-MC3HP and HVP-KV46F150M development board. I want some Project examples (MCUXpresso and FreeMaster) based on motor driver.

Can you share some project examples 

0 件の賞賛
返信
3 返答(返信)

3,099件の閲覧回数
harsh_kumbhar
Contributor I

Thank You,

I got example in SDK 

while using example in freemaster it is showing missing symbol veriable how to handle it 

pastedImage_1.png

0 件の賞賛
返信

3,099件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

 

You need to select the .axf file as follows.

 

In Freemaster go to Project > Options and then click the MAP files tab. Then in Default symbol file select your .axf generated in the Debug folder of your SDK project.

 

Finally select File format as Binary ELF. Please check the snippet below.

pastedImage_8.png

Best regards,

Felipe

0 件の賞賛
返信

3,099件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello,

 

The examples we provide are located in their corresponding SDK package. You can download the examples from the link below.

Welcome | MCUXpresso SDK Builder 

 

You need to download the SDK for HVP-KV46F150M. There you will find motor control examples that uses HVP-MC3PH platform.

 

I hope this helps!

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信