PMSM FOC control with position sensor (encoder)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMSM FOC control with position sensor (encoder)

Jump to solution
5,583 Views
peterkostadinov
Contributor III

Hi All,

I need example project with PMSM FOC control, but with position sensor (encoder), instead of available examples, which are SENSORLESS.

Best Regards,

Peter

0 Kudos
Reply
1 Solution
5,202 Views
philip_drake
NXP Employee
NXP Employee

Please see this Application Note: 

    • AN12374

There is an encoder project in the software package as well as a hall effect start-up FOC software project.

Regards,

Philip

View solution in original post

4 Replies
5,202 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Peter,

Besides the FRDM-KV31 solution for PMSM FOC control based on encoder sensor as Philip pointed out, this is the DSC solution. Pls download "PMSM_FOC_ENCODER_MC56F84789_TWR_DEMO" from the following link:

PMSM FOC Industrial Drives Reference Design | NXP 

Hope it can help you

BR

XiangJun Rong

5,202 Views
peterkostadinov
Contributor III

Thank you very much for your support!

Best Regards,

Peter

0 Kudos
Reply
5,203 Views
philip_drake
NXP Employee
NXP Employee

Please see this Application Note: 

    • AN12374

There is an encoder project in the software package as well as a hall effect start-up FOC software project.

Regards,

Philip

5,202 Views
peterkostadinov
Contributor III

Thank you very much for your support!

Best Regards,

Peter

0 Kudos
Reply