MKM34Z256XX7 Flash problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MKM34Z256XX7 Flash problem

跳至解决方案
3,225 次查看
avinashbhavsar
Contributor I
kinetic series MKM34Z256VLQ7 Flash problem
I am successfully  able to access the flash and save data with creating memory blocks.
But  at the time of  erase memory block individually, The whole memory with all blocks are erase same time.
As per  application, Memory of single block has to clean and update as per the function used.
Please help with the same .
thank you .
标签 (1)
0 项奖励
回复
1 解答
3,083 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Avinash Bhavsar,

  It seems this post is the same question as this post:

https://community.nxp.com/message/1062488?commentID=1062488#comment-1062488 

  And I already answer that question in that post, you can refer to it directly.

   If you still have question about it, welcome to let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,084 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Avinash Bhavsar,

  It seems this post is the same question as this post:

https://community.nxp.com/message/1062488?commentID=1062488#comment-1062488 

  And I already answer that question in that post, you can refer to it directly.

   If you still have question about it, welcome to let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,083 次查看
avinashbhavsar
Contributor I

Thank you Kerry,

I had solve that problem  ,I use RAM while clearing flash then reload new data with addition of old data  to flash .

Avinash.

0 项奖励
回复