MCDRV_QdEncGet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCDRV_QdEncGet

3,470 次查看
FaustoPignatta
Contributor I

Hi,

in this function I find this piece of code

/* tracking observer calculation */
this->f16PosMeEst = (frac16_t)AMCLIB_TrackObsrv_A32af(this->a32PosErr, &this->sTo);

My question is: why use AMCLIB_TrackObsrv_A32af library function if we read the signal from encoder?

Also the speed seem to be "estimated"

/* speed estimation by the tracking observer */
this->fltSpdMeEst = this->sTo.fltSpeed;

Thanks,

Fausto

0 项奖励
回复
7 回复数

3,337 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

The code located at <mcdrv_enc_qd.c> file MCDRV_QdEncGet() function, which is related driver for encoder.

The AN12659 provides the detailed info about hardware connections:

Hui_Ma_0-1651736400749.png

Hui_Ma_1-1651736473531.png

Hui_Ma_2-1651736586730.png

 

Thank you for the attention.

Mike

0 项奖励
回复

3,466 次查看
nxf45548
NXP Employee
NXP Employee

Thank you for contacting NXP technical support. 
To provide you with better support, can you please let us know the part number you are using?
Are you using an S32K, KE, LPC800, etc? 

0 项奖励
回复

3,461 次查看
FaustoPignatta
Contributor I

Hi,

I'm using ImxRt1050 with the quad motor control develpment platform.

The version of SDk is 2.11.0.

Thank you,

 

0 项奖励
回复

3,401 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Could you help to provide the demo name or demo location at RT1050 SDK V2.11.0 package? Thanks.

Mike

 

0 项奖励
回复

3,388 次查看
FaustoPignatta
Contributor I

Hi,

it isn't a project from 2.11 sdk version. The project name is Quad-Motor-Control-FreeMASTER-Project-Sample-Project.

Thanks,

Fausto

0 项奖励
回复

3,371 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Thank you for the info.
I am in progress to get related demo codes be downloaded and will check related project later.
Thank you for the patience.

Hui_Ma_0-1651222184244.png

Mike

0 项奖励
回复

3,455 次查看
nxf45548
NXP Employee
NXP Employee

Thank you for the clarification.
I'll redirect the inquiry to our product specialist and they could further assist you. 

0 项奖励
回复