EB Tresos 16.0 code generation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EB Tresos 16.0 code generation

2,322 Views
LucaOlivero
Contributor I

Hi all,

I am trying to configure TLF35584 with EB Tresos. I inserted the modules SafeWdgExtTlf v0.0.1 - AS3.2.1 and SafeWdgQspi v.0.0.1 - AS3.2.1. The verification and generation phases end correctly but the output code doesn't compile. The strange thing is that the SafeWdgExtTlf_PBCfg.c doesn't include the corresponding .h (SafeWdgExtTlf_Cfg.h). Moreover the SafeWdgExtTlf_PBCfg.c uses "SafeWdgExtTlf_ConfigType" without include the .h that define that struct (SafeWdgExtTlf.h). If I manually include all the necessary .h the compilation ends correctly.

In attach you can find the generated files.

Thanks in advance

Luca

0 Kudos
Reply
2 Replies

2,293 Views
LucaOlivero
Contributor I

Thank you so much for the answer.

Best Regards,

Luca

0 Kudos
Reply

2,296 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

Unfortunately, I'm afraid that we couldn't help, as TLF35584 is provided by Infineon, not NXP, and we don't have the driver for TLF35587 available.

Best Regards,

Nam

0 Kudos
Reply