BEMF observer(AB axis – F16) in RTCSEL Library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BEMF observer(AB axis – F16) in RTCSEL Library

2,725 Views
muthus
Contributor I

Hi,

For our motor control application, We are using a Back EMF observer to measure the speed of the motor. There are two types of Backemf observers(AB axis, DQ axis) are available. We need to use the observer with AB axis for our application. We found that observer(BEMF AB axis ) is not working as expected.
The problem is that the "estimated backemf voltage(sEObsrv) and estimated current (sIObsrv) are getting saturated at negative maximum value immediately and the output structure(sUnityVctr) always shows Frac16(0.707). We have set up the gain values as per given in AMCLIB user guide section 2.6.2. And we have tried with different set of gain values, still the problem continues.

Microcontroller : Kinetis MKV30VLF10P
Library : RTCSEL v4.5
Backemf Observer : AB axis (F16)

Regards,

Muthu S

0 Kudos
Reply
1 Reply

2,487 Views
pavelsustek
NXP Employee
NXP Employee

Hi Muthu S,

follow please thus thread: https://community.nxp.com/thread/496636, where the same issue has been solved.

Regards,

Pavel

0 Kudos
Reply