BEMF observer(AB axis – F16) in RTCSEL Library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BEMF observer(AB axis – F16) in RTCSEL Library

2,692件の閲覧回数
muthus
Contributor I

Hi,

For our motor control application, We are using a Back EMF observer to measure the speed of the motor. There are two types of Backemf observers(AB axis, DQ axis) are available. We need to use the observer with AB axis for our application. We found that observer(BEMF AB axis ) is not working as expected.
The problem is that the "estimated backemf voltage(sEObsrv) and estimated current (sIObsrv) are getting saturated at negative maximum value immediately and the output structure(sUnityVctr) always shows Frac16(0.707). We have set up the gain values as per given in AMCLIB user guide section 2.6.2. And we have tried with different set of gain values, still the problem continues.

Microcontroller : Kinetis MKV30VLF10P
Library : RTCSEL v4.5
Backemf Observer : AB axis (F16)

Regards,

Muthu S

0 件の賞賛
返信
1 返信

2,454件の閲覧回数
pavelsustek
NXP Employee
NXP Employee

Hi Muthu S,

follow please thus thread: https://community.nxp.com/thread/496636, where the same issue has been solved.

Regards,

Pavel

0 件の賞賛
返信