AMCLIB_ACIMRotFluxObsrv input parameters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AMCLIB_ACIMRotFluxObsrv input parameters

Jump to solution
3,520 Views
General_motor_control
Contributor II

We have a three-phase induction machine (IM), of which we want to know the following motor parameters:

Rs:            stator resistance [Ohm]

Ls:             stator inductance [Henry]

Lm:           magnetizing inductance [Henry]

Rr:             rotor resistance [Ohm]

Lr:              rotor inductance [Henry]

For sensorless control of the IM, we use the AMCLIB_ACIMRotFluxObsrv and AMCLIB_ACIMSpeedMRAS. Rs and Ls are measured and verified - thus certain. However, executing the no-load and blocked-rotor test results in Lm >> Lr, Ls (magnetizing inductance greater than the product of stator- and rotor-inductance), which seems legit comparing to other papers and/or results found online. However, fltKrLsTotLeakGain from the AMCLIB_ACIMRotFluxObsrv ends up to be a negative gain in this way as the formula is:

((Lr * Ls) - Lm^2) / Lm

This seems to be faulty? Because a negative gain will not work out. What could be a possible cause?

 

0 Kudos
Reply
1 Solution
3,432 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @General_motor_control ,

He knows more about motor control software libraries. You should trust him. I only analyzed based on the T-equivalent circuit, so my view might not cover everything. Sorry for that.

BRs,

Celeste

View solution in original post

0 Kudos
Reply
5 Replies
3,440 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @General_motor_control ,

Thanks for your post.

I believe that there is something wrong with your understanding. In the T-equivalent circuit, there is the following formula. For example, in the (PDF) On the Identifiability of Steady-State Induction Machine Models Using External Measurements

 

Screenshot 2025-03-07 171946.png

The Lm is the mutual equivalent inductance, it should be less than Ls, Lr. So the fltKrLsTotLeakGai formula in document CM7FAMCLIBUG.pdf is correct. Please check your parameter definition or test method.

Hope it can help you.

 

BRs,

Celeste

0 Kudos
Reply
3,437 Views
General_motor_control
Contributor II

Hello @Celeste_Liu 

 

Please find the answer of another NXP employee on my question through the following link: https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/AMCLIB-ACIMRotFluxObsrv-input-parameter... 

What are your thoughts on this? We were redirected to this forum.

 

Kind Regards,

 

3,433 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @General_motor_control ,

He knows more about motor control software libraries. You should trust him. I only analyzed based on the T-equivalent circuit, so my view might not cover everything. Sorry for that.

BRs,

Celeste

0 Kudos
Reply
3,501 Views
Veronika_techsupport
NXP TechSupport
NXP TechSupport

Hello @General_motor_control 

could you please clarify what particular NXP product you reffered to? 

Model Based Design Tools (MBDT) are supported by our MBDT experts via NXP technical community only.

Could you please submit a new community thread here: https://community.nxp.com/community/mbdt 
 
Our experts will gladly help you there.
0 Kudos
Reply
3,497 Views
General_motor_control
Contributor II

Dear Veronika,

We use an MKV58 on a custom PCB. So no specif MBDT. However, we do use the standard NXP libraries from the AMCLIB - as mentioned previously - the AMCLIB_ACIMRotFluxObsrv and AMCLIB_ACIMSpeedMRAS. 

Document: https://www.nxp.com/docs/en/user-guide/CM7FAMCLIBUG.pdf

Kind Regards,

 

0 Kudos
Reply