who can give a sample and explain process of LIN example run on s32k1xx EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

who can give a sample and explain process of LIN example run on s32k1xx EVB

2,463 Views
642142357
Contributor III

need:

1. build a *.ldf and *.npf sample file with code warrior above 10.0 version .

2. generated program files lin_cfg (lin_cfg.c,lin_cfg.h,lin_hw_cfg.h) will be amend with  uart port of s32k144 and integrate them  into a sample project in s32k144 example and run it on the  s32k1xx EVB board. the sample as sample as possible ,only to show the function of lin send and receive  message.

3. use a monitor gui software on the personal computer such as CANcaseXL and so on ,to show the send or receive message .

who can provide this sample ,thanks very much.johnsen_zhouwjandsqkhumphriMandardhavalRHinnen

Labels (4)
0 Kudos
Reply
1 Reply

2,411 Views
constantinrazva
NXP Employee
NXP Employee

Hello 642142357@qq.com ,

Unfortunately on this community we only handle question regarding MATLAB/Simulink and our toolboxes. If you want to use our toolbox for S32K1xx family (in Simulink - link kere) you'll find there an example for LIN. Otherwise I would sugest you post your question on S32K  community.

Kind regards,

Razvan.

0 Kudos
Reply