trouble using freeMaster with S32m24x_pmsm_Sensorless example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

trouble using freeMaster with S32m24x_pmsm_Sensorless example

789 次查看
ParisaShams
Contributor I

Hi, 

I am running the sensorless example and I would like to see variables in freeMASTER. If I add new variables in the simulink as Volatile objects then the logged signals in freeMaster keep switching from "?" to "their value" and back to "?" ...
I found out if I only add one more variable, it runs fine but if I add more I get this weird behavior. I see the motor is running but data logging and monitoring keeps going to "?" Is there a limitation on number of variables/signals? How can I resolve this? Thanks

ParisaShams_0-1739304247672.png

ParisaShams_2-1739304270238.png

ParisaShams_1-1739304262831.png

 

 

标记 (3)
0 项奖励
回复
0 回复数