trouble using freeMaster with S32m24x_pmsm_Sensorless example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

trouble using freeMaster with S32m24x_pmsm_Sensorless example

750件の閲覧回数
ParisaShams
Contributor I

Hi, 

I am running the sensorless example and I would like to see variables in freeMASTER. If I add new variables in the simulink as Volatile objects then the logged signals in freeMaster keep switching from "?" to "their value" and back to "?" ...
I found out if I only add one more variable, it runs fine but if I add more I get this weird behavior. I see the motor is running but data logging and monitoring keeps going to "?" Is there a limitation on number of variables/signals? How can I resolve this? Thanks

ParisaShams_0-1739304247672.pngParisaShams_0-1739304247672.png

ParisaShams_2-1739304270238.pngParisaShams_2-1739304270238.png

ParisaShams_1-1739304262831.pngParisaShams_1-1739304262831.png

 

 

タグ(3)
0 件の賞賛
返信
0 返答(返信)