the eTimer module configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

the eTimer module configuration

3,173 次查看
hjhjhj
Contributor IV

Hi Daniel,

        I try to configure the eTimer module to read more input pins,such as A4,A5,A6,A7,A8,F0 and D14.But only the input pin A0 is availble.It's possible that there's some problem in my configuration.Can you help me find it?The HW I used is MPC5744P DevKit.

 

Thanks!

Hj

0 项奖励
回复
3 回复数

2,954 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello hjhjhj‌,

Let's try like this: please replace in the {Path where you installed the toolbox}\mbdtbx_pnt\src\c_library the .c attached file (an advice would be to rename the existing one and keep it  in case the one provided is not ok) and then try to test your model or the one attached.
I'm looking for your response to see if this worked or not.

Hope that helps, 

Marius

0 项奖励
回复

2,954 次查看
hjhjhj
Contributor IV

Hello Marius,

      Sorry for delay.The model  attached work,but the pins A0,F0,D14,A4 always work at the same time and the any of pins A5,A6,A7,A8 affects the four pins A0,F0,D14,A4 .Is there any solutions for this.

Thanks!

Hj

0 项奖励
回复

2,954 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi hjhjhj

We are looking into this. Stay tuned - we will update soon!

Thank you!

Daniel

0 项奖励
回复