target configuration problems for s32k in PIL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

target configuration problems for s32k in PIL

2,462件の閲覧回数
geertvenken
Contributor I

When starting the PIL testing of a model with test harness, following error appears:

Cannot perform a processor-in-the-loop (PIL) simulation for "State_Machine". The configuration parameters for this model do not support the following connectivity configurations: Texas Instruments Code Composer Studio (IDE), Texas Instruments Code Composer Studio (TCP/IP), Texas Instruments Code Composer Studio (Serial), s32k_pil PIL, s32k_as_pil PIL To fix this error, update the configuration parameters or create a supported connectivity configuration. See Configure a SIL or PIL Simulation, Create a Connectivity Configuration for a Target, and Processor-in-the-Loop (PIL) Simulation in your product help.

S32k configuration block is present and PIL option is selected.

There is a workaround , remove the s32k configuration block from the model and place it back.  Restart the SIL and everything works fine.

Took me 2 days to fined this simple hack.

But this is not a real solution as the problem pops-up again after re-opening the project.

0 件の賞賛
返信
2 返答(返信)

1,948件の閲覧回数
geertvenken
Contributor I

the S32 configuration block must be added in every model, not only in the top view

0 件の賞賛
返信

2,004件の閲覧回数
pierpaolo_dini
Contributor III

@geertvenken 

Since i face the same problem, i ask if you solve in some way!
Thank you!

Pierpaolo.

0 件の賞賛
返信