s32k344 generate code error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k344 generate code error

1,558 Views
ca_liu
Contributor II

It's something wrong happened when I tried to generate code with s32ct for s32k344(footprint bga257),fault details are shown in the figure.And it seems to be related to the can module.When I delete the can module, the code can be generated normally, and the fault occurs again after adding it.

The version of s32ct is 1.4r,and it‘s installed automatically with mdbt (MBDToolbox_S32K3xx_1.1.0_20211220.mltbx)。

I hope I can get some help,thanks very much.

Tags (1)
0 Kudos
Reply
0 Replies