s32ct generate code error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32ct generate code error

1,846 Views
ca_liu
Contributor II

It's something wrong happened when I tried to generate code with s32ct,fault details are shown in the figure.And it seems to be related to the can module.When I delete the can module, the code can be generated normally, and the fault occurs again after adding the module.

The version of s32ct is 1.4r,and it‘s installed automatically with mdbt (MBDToolbox_S32K3xx_1.1.0_20211220.mltbx)。And the chip is s32k344,footprint bga257.

I hope I can get some help,thanks very much.

Tags (1)
0 Kudos
Reply
0 Replies