s12zvm MBD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s12zvm MBD

827 Views
SpencerYu
Contributor I

We got some issues when we configuration the MBD ,May you help to guide us fixed it?

 

Problems with automatic code generation using S12ZVMX MBD toolbox
1 System clock cannot be configured to 16MHz
2 .c contains wrong header file, even if it is not generated (not supported for compact style code)
3 Model compilation cannot find predefined files
4 LIN interrupt interface is not compatible
5 LIN lacks set idle, wakeup function interface
6 LIN interface data type is uint16, and the base software in uint8 does not match the problem
7 LIN initializes the register  miss the interrupt  registers  configuration

8 no need register configuration case, how to read the value of the MCU register
9 Timer configuration, no channel_0, cannot configure the system clock
10 ADC system default clock is 50MHz, cannot be modified
11 ADC does not detect the conversion completion flag without using interrupts
12 How to use the others defined MCU registers
13 CPU module only contains the basic clock configuration, no peripheral initialization, and the basic software compatibility is difficult

0 Kudos
Reply
0 Replies