s-function builder

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s-function builder

2,557 Views
saurabhkulkarni123
Contributor II

Hi, 

I have LED blinking code of s32k148, now I want to build custom block for that I have to port this code in S-function builder block and generate TLC file for same. I want know about procedure for this and also want to know about which files are required for building in s-function builder.

0 Kudos
Reply
2 Replies

2,554 Views
Martha09
Contributor I

To build a custom S-function block in Simulink's S-function Builder, you can Prepare the code, Creation an S-function project, Define S-function parameters, Implement S-functions methods, Configure S-function builder, Build the S-function, test and Deploy.

0 Kudos
Reply

2,546 Views
saurabhkulkarni123
Contributor II
I have code where Pin are assign to led, but in s-function builder how can I declare pin.
0 Kudos
Reply