problems with Gpt Notification 358 EBT example project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

problems with Gpt Notification 358 EBT example project

1,952 次查看
XH
Contributor I

Hi there,

 

I encountered this problem with deploying the project " Gpt Notification 358 EBT example" to S32K358 processor, as shown in the attached image.

 

Could you please help?

 

Many thanks,

 

Xiaomei

0 项奖励
回复
1 回复

1,914 次查看
FlorinCiuca
NXP Employee
NXP Employee

Hello @XH !

 

From what I can see from the attached screenshot, it seems that the model you are trying to build is placed at a wrong path (C:\Users).

folder.png

It is very likely that you(or MATLAB) do(does) not have the correct privileges/write access in C:\Users. Please try to move the model at the path where your MATLAB projects are stored and re-build from there. Or if you did not make any changes to the model, you can try to build it directly from the Examples folder of the toolbox.

Best regards,

Florin.

0 项奖励
回复