port pin configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

port pin configuration

1,379 Views
paul_ephraim_13
Contributor III

paul_ephraim_13_0-1726810362124.png

i am unable to understand what the PortPin id is all about and the way it is numbered.
Please clarify and suggest some step by step configuration manual from scratch to build a basic model for s32k312 

Tags (1)
0 Kudos
Reply
1 Reply

1,361 Views
dragostoma
NXP Employee
NXP Employee

Hi, @paul_ephraim_13 

As I explained in the previous post, the number chosen for the PortPin Id section can be chosen randomly, but within the range of the number of configured pins: if you have 5 configured pins, IDs can be randomly chosen between 1-5, i.e. you can have either 1 2 3 4 5 or 3 2 4 1 5, it doesn't matter. As long as the IDs are in the range of configured pins, everything will work correctly. If, for example, you will put ID 6 to one of the pins, you will encounter the initial problem you had, due to you can't have the value of the PortPin Id greater than the number of defined pins.

In the configuration of the pins, this ID is just a symbolic number, which you can interpret as an index of the pins. What is important in configuring the pins is the PortPin Mscr, which is chosen based on the board's hardware schematic.

I hope this clears up your confusion.

 

Best regards,

Dragos

0 Kudos
Reply