no licence activation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

no licence activation

Jump to solution
1,026 Views
bryce1
Contributor I

Hello

I have a problem with the activation of the licence for the Model Based Design ToolBox 

I download the licence file and tried to activate with the 

Model Based Design Toolbox Installation guide, but it don't work

I gave my host ID from the command line VOL in the CmD on Windows

Is it possible to save the problem 

Thanks

0 Kudos
Reply
1 Solution
970 Views
dragostoma
NXP Employee
NXP Employee

Hi, @bryce1,

So you are using the S32K1 toolbox, version 4.3 in MATLAB 2024a, and you have managed to activate the license.
First, make sure that the MATLAB path is correct and ready for using the toolbox, by running the script mbd_s32k_path.m from the src folder. This way, all the files and folders necessary for using the toolbox are added to the MATLAB path.

 
 
 
 

image.png


The error you reported is related to the configuration block, where the parameters are not recognized.
After running the path script and the problem still persists, I would like you to detail the steps you followed until you encountered this error, in order to investigate possible causes of the problem, namely:
- which model did you open
- if you modified anything in the blocks and what exactly did you modify
- additional actions you took


Let us know how the process works.

 

Best regards,

Dragos

View solution in original post

0 Kudos
Reply
3 Replies
1,000 Views
bryce1
Contributor I

Hi, I'm using the 4.3 version of the toolbox, with matlab 2024a

When I tried to activate and to verify the licence, there are 2 messages :

first one : NXP Model-Based Design Toolbox for S32k1xx licence activation was succesfull

second one : Dot indexing is not support for variable of this type

Nevertheless, when I tried to compile a simulink model, there are many message about missing parameters of MBDTBX_EC_S32K-AS block

Thanks

Bryce

0 Kudos
Reply
971 Views
dragostoma
NXP Employee
NXP Employee

Hi, @bryce1,

So you are using the S32K1 toolbox, version 4.3 in MATLAB 2024a, and you have managed to activate the license.
First, make sure that the MATLAB path is correct and ready for using the toolbox, by running the script mbd_s32k_path.m from the src folder. This way, all the files and folders necessary for using the toolbox are added to the MATLAB path.

 
 
 
 

image.png


The error you reported is related to the configuration block, where the parameters are not recognized.
After running the path script and the problem still persists, I would like you to detail the steps you followed until you encountered this error, in order to investigate possible causes of the problem, namely:
- which model did you open
- if you modified anything in the blocks and what exactly did you modify
- additional actions you took


Let us know how the process works.

 

Best regards,

Dragos

0 Kudos
Reply
1,005 Views
dragostoma
NXP Employee
NXP Employee

Hi, @bryce1,

First of all, which toolbox in the Model Based Design suite are you using and what is the error you are encountering? Because based on the error displayed we can figure out the cause of the problem that led to this error.

Until you help us with the error displayed, I advise you to read a similar thread that might help you in the license activation process: https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Unable-to-active-MBD-Toolbox/m-p/195501...

 

Best regards,

Dragos

0 Kudos
Reply