license error -1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,881件の閲覧回数
lethuer2
Contributor II

Hi,

I have some trouble with the license file.

I generated a license file with my host id, which is shown here:

1.PNG

The generated license.dat file is stored in the correct directoty:

2.PNG

The toolbox is installed in the standard folder: C:\MCToolbox

The path is setted correctly:

>> mcd_kv_path
Treating 'C:\MCToolbox\mctbx_Kinetis' as MCD Toolbox installation root.
MCD Toolbox path prepended.
Successful.

But I still get this error message while building the model:

3.PNG

I have restarted MATLAB and windows.
Please give me some instructions... I don't have any idea anymore.

0 件の賞賛
返信
1 解決策
2,677件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi lethuer‌,

Can you please change the license file extension from .dat into .lic

That should make it work.

Hope it helps!

Daniel

元の投稿で解決策を見る

2 返答(返信)
2,678件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi lethuer‌,

Can you please change the license file extension from .dat into .lic

That should make it work.

Hope it helps!

Daniel

2,677件の閲覧回数
lethuer2
Contributor II

You are right !

Thank you very much :smileyhappy:

0 件の賞賛
返信