license error -1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

license error -1

Jump to solution
5,875 Views
lethuer2
Contributor II

Hi,

I have some trouble with the license file.

I generated a license file with my host id, which is shown here:

1.PNG

The generated license.dat file is stored in the correct directoty:

2.PNG

The toolbox is installed in the standard folder: C:\MCToolbox

The path is setted correctly:

>> mcd_kv_path
Treating 'C:\MCToolbox\mctbx_Kinetis' as MCD Toolbox installation root.
MCD Toolbox path prepended.
Successful.

But I still get this error message while building the model:

3.PNG

I have restarted MATLAB and windows.
Please give me some instructions... I don't have any idea anymore.

0 Kudos
Reply
1 Solution
2,671 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi lethuer‌,

Can you please change the license file extension from .dat into .lic

That should make it work.

Hope it helps!

Daniel

View solution in original post

2 Replies
2,672 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi lethuer‌,

Can you please change the license file extension from .dat into .lic

That should make it work.

Hope it helps!

Daniel

2,671 Views
lethuer2
Contributor II

You are right !

Thank you very much :smileyhappy:

0 Kudos
Reply