Hello, @Sam_ECU
Even if we do not support the profiling blocks, I have a sort of approach to measure execution time. For this, you can use the GPT, which is an up-counting timer. The workflow on code perspective would be this:
GPT_StartTimer(GPT_instance);
/* code_to_be_measured */
ticks = GPT_GetCurrentTimerCount(GPT_instance);
GPT_StopTimer(GPT_instance);
So you can put your algorithm you want to measure the time of execution in a subsystem, then you have to add the blocks for starting and stopping the GPT and the Timer Counter Value block to get the ticks from the timer.
stefancinipeanu_1-1653044007064.png
In Simulink, to generate the code in the way described upper, you have to put priorities to the blocks. So the TimerStart block has priority 0, Subsystem_To_Measure has priority 1, TimerCounterValue block has priority 2 and TimerStop block has priority 3. To put priorities for each block/subsystem, you have to right-click on a block/subsystem, go to Properties... and introduce the priority in the Priority field.
stefancinipeanu_0-1653043934517.png
In the mex file attached to the model, you have to set the GPT timer to run in Free Run Mode in order to let the Timer to count to the maximum value (0xFFFFFFFF) and also enable Reset counter when re-enabled checkbox in order to reset the current counter value to 0 when the GPT_StopTimer function is called.
stefancinipeanu_2-1653044387815.png
The current counter value is put in ticks data memory store and it can be visualized in the FreeMASTER project attached.
I have also attached the model. You can check it and see if it suits for your application.
Hope this helps.
Regards,
Stefan.