iMXRT: ASAP2 Interface with If_Data and A2ML

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT: ASAP2 Interface with If_Data and A2ML

2,245 Views
Sam_ECU
Contributor V

Hello,

I'm trying to tune the iMXRT with code from MBDT with external software (INCA / CANape etc.)

The MBDT for iMXRT supports XCP Communication (Serial and Ethernet) within Simulink and therefore with third party software.

The next step is to generate the A2L file.  Under "Code Generation - Interface" the "ASAP2 Interface" can be selected.  When building the model it exports the A2L file, but the A2ML and If_Data Sections are missing. Signals and Parameters are exported.

How to export or find the correct XCP server configuration which is being using by MBDT for XCP?

When trying to use the Matlab functionality, it appears certain information is missing from the generated code folder:

https://ch.mathworks.com/help/releases/R2022b/rtw/ref/coder.xcp.a2l.addcoderxcpinfo.html

I couldn't get another option provided by Simulink to work with the iMXRT MBDT either:

https://ch.mathworks.com/help/rtw/ug/calibrate-generated-code-and-monitor-signals-via-xcp-and-third-...

Regards,

Sam

0 Kudos
Reply
2 Replies

2,016 Views
Sam_ECU
Contributor V

Hello NXP,

Could I receive help with the issue?

Tags (1)
0 Kudos
Reply

2,175 Views
Sam_ECU
Contributor V

Hello NXP,

Could I receive help with the issue?

0 Kudos
Reply