iMXRT: ADC_ETC Configuration Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT: ADC_ETC Configuration Problem

1,026 Views
Sam_ECU
Contributor V

Hello,1

I'm working with iMXRT1062 and can't get ADC2_IN1 (Pin H12) to correctly read a voltage input using ADC_ETC in MBDT.

In total I'm measuring 12 pins and I only have issues with ADC2_IN1, the other pins measure fine.  I'm also measuring most of the pins in ADC1 and a higher sample rate.

The setup is based off the example "ADC_ETC_Hardware":

Sam_ECU_0-1720008984427.pngSam_ECU_0-1720008984427.png

I can measure on the pin with a multimeter and there is no issue in the hardware.  I can also take the "ADC_Polling" example and measure on ADC2_IN1 without issue.  I know the issue is in the software and not in the hardware.

 

What is the issue in my setup using ADC_ETC?

Attached my config files based off "ADC_ETC_Hardware" and "ADC_Polling"

0 Kudos
Reply
1 Reply

932 Views
Sam_ECU
Contributor V

Hello @stefancinipeanu 

Are you potentially the right person to help me with this issue?

0 Kudos
Reply