how to build program generated by mbd Toolbox in the keil?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to build program generated by mbd Toolbox in the keil?

1,790 Views
642142357
Contributor III

how to setup a project or  build  program  generated by  mbd Toolbox in the keil5?  constantinrazvan.chivu

Labels (1)
Tags (1)
2 Replies

1,694 Views
constantinrazva
NXP Employee
NXP Employee

Hello 642142357@qq.com,

Unfortunately we do not have support for exporting projects generated from our toolbox to Keil5 uVision 5 IDE - if you want to bring it there, you'll have to manually set it up (copy the files would be easy, but you'll also have to set the linker files to be used, etc.). The only IDE that we export to is S32Design Studio - for that you'll do a simple import and you'll have everything set-up.

Kind regards,

Razvan.

1,694 Views
mariuslucianand
NXP Employee
NXP Employee

Hello 642142357@qq.com‌,

The only suggestion I have, in addition to what constantinrazvan.chivu recommended to you, is once you have imported the code in S32DS, to export it to be used for Keil. Maybe this link can help you Using Keil μVision 5 with Processor Expert | MCU on Eclipse 

Hope this helps,

Marius

0 Kudos
Reply