floating to fixed point conversion-help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

floating to fixed point conversion-help

1,326 Views
garimella
Contributor I

I was referring to AN3943 - which provides details of ATO algorithm. We require to generate C code using HDL coder from simulink to flash to the target(kinetis). We tried first by modelling this algorithm in simulink using all floating point operations. It works fine. Next we wanted to convert this to fixed point and we got into trouble. We are using external ADC(AD7606) to read the quadrature inputs. So we fixed the input data type to fixdt(1,16,15). sine/cosine functions within simulink was used. The results after fixed point conversion is erratic. Please provide advise for the same.

0 Kudos
Reply
0 Replies