devkit MPC5744P communication test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

devkit MPC5744P communication test

ソリューションへジャンプ
4,531件の閲覧回数
henryex2009
Contributor I

 Hi everyone,

 I used MPC5744P to test UART . I successfully download the "Hello word" example to the DEVKIT 5744P

through this MBT tool(Version 3.2),but the Tera Term show nothing. Please tell me how to solve this problem.

BTW, the CAN commuication example also has same problem.The model is download into DEVKIT 5744P,but I can't see the CAN RX/TX( by INCA).

0 件の賞賛
返信
1 解決策
4,445件の閲覧回数
hbhnhbnhj1
Contributor III

Hi @henryex2009,

You can change the serial port to 0 as shown in figure below, it should work.

hbhnhbnhj1_0-1650447710662.png

 

元の投稿で解決策を見る

タグ(3)
0 件の賞賛
返信
3 返答(返信)
4,446件の閲覧回数
hbhnhbnhj1
Contributor III

Hi @henryex2009,

You can change the serial port to 0 as shown in figure below, it should work.

hbhnhbnhj1_0-1650447710662.png

 

タグ(3)
0 件の賞賛
返信
4,405件の閲覧回数
henryex2009
Contributor I

Hi,hbhnhbnhj1,

It works,thank you for your assistance

0 件の賞賛
返信
4,398件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @henryex2009

Please have a look at the Schematics of the EVBs before developing your application, to make sure that the right pins are selected inside the blocks, alongside the right UART instances.

https://www.nxp.com/design/development-boards/automotive-development-platforms/mpc57xx-mcu-platforms... 

Hope this helps,

Marius

0 件の賞賛
返信