Why is the UART in Coordinator not working properly in JN5169?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why is the UART in Coordinator not working properly in JN5169?

1,280件の閲覧回数
1979717461
Contributor III

I created the UART in the Coordinator, but it doesn't work. For example, I send 0xFF through the serial port. However, the content received by the serial port assistant is 0x3F. When sending 0, the serial port cannot receive it. But creating the same UART works fine in EndDevice.I do not know why it has to be like this.

Have you ever encountered this situation? thank you very much for your reply.

タグ(2)
0 件の賞賛
返信
1 返信

1,231件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello 1979717461@qq.com‌,

Unfortunately on this community we only handle issues regarding MATLAB/Simulink and our toolboxes. I would suggest to post this question in the https://community.nxp.com/community/wireless-connectivity .

Hope this helps,

Razvan.

0 件の賞賛
返信