Why MBD ToolBox just only one "Timer block"?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why MBD ToolBox just only one "Timer block"?

2,761件の閲覧回数
niequanwei
Contributor III

When I used the MBD ToolBox ,I just find that there was only one "Timer Block" 

1.jpg

However, the reference manual sheet has two timers.

2.jpg

Meanwhile, there are many registers, and I just don't know how to configure it from the that block,such as"How to select one of the timers" and so on.

タグ(4)
2 返答(返信)

2,639件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

This is an older toolbox and it only supports one timer block. Unfortunately we do not have a newer version for the MCU you are using. Our newer releases (like S32K14x) support many more peripherals, so if that's of interest to you, please take a look.

Kind regards,

Razvan.

2,639件の閲覧回数
niequanwei
Contributor III

Got it ! Thank you!

0 件の賞賛
返信