Where can i get the program which used in MTRCKTDPS5643L board to test it?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can i get the program which used in MTRCKTDPS5643L board to test it?

1,993 Views
edenli
Contributor V

Hi Guys,

    i bought the MTRCKTDS5643L board from NXP,but i just received the board,there isn't the program to test the board,Where can i get the code to down load in it to make the dual PMSM running?

6 Replies

1,800 Views
petrfajmon-b173
NXP Employee
NXP Employee

Hi Eden Li, Daniel

  currently, we were finalized the new version of the software for the dual 3-phase PMSM Development Kit with NXP MPC5643L MCU v1.1. The new version of the Motor Control DevKit SW package supports S32 Design Studio for Power IDE v1.1, SW package can be downloaded here:

http://www.nxp.com/downloads/en/apps/MTRCKTDPS5643L_SW.exe  

Best Regards,

Petr

1,800 Views
edenli
Contributor V

Hi Petr,

Thank you for your reply!

Best Regards!

Eden Li

0 Kudos
Reply

1,800 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi edenli

This is the only SW i can find on NXP webside related with this product: Dual 3-phase PMSM Kit with MPC5643L MCU|NXP . It is a C-source like project.

Capture.PNG

0 Kudos
Reply

1,800 Views
edenli
Contributor V

Hi Daniel,

I down load it and running,finding that it is not a project,i do not know how to use it?

if NXP provide a project of Codewarior?

0 Kudos
Reply

1,800 Views
Daniel_Popa
NXP Employee
NXP Employee

To be honest - i'm not familiar with these development kits.

petrfajmon-b17364‌,

Do you know anything about this development kit: MTRCKTDPS5643L: Dual 3-phase PMSM Development Kit with NXP MPC5643L MCU ? Can you point us to a person that might be familiar with ?

Thank you!

Daniel

 

1,800 Views
edenli
Contributor V

Hi Daniel.

Thank you for your reply!

Best Regards!

Eden    Li

0 Kudos
Reply