What CAN channels are Supported by Simulink on the dev board X-RDVCU5775EVM Ver B?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What CAN channels are Supported by Simulink on the dev board X-RDVCU5775EVM Ver B?

613 次查看
ranulf
Contributor IV

I am using:

  • Windows 10
  • MATLAB/Simulink 2020a
  • MBDT version 3.2.0
  • The dev board X-RDVCU5775EVM Ver B, which has the MPC5775B chip

With the target set at MPC5777C in the 'MBD_MPC574x_Config_Information' block I have only been able to get one of the CAN channels to work:

  • In Simulink: 'FCAN Module: 0'
  • On the 130-pin ECU Cable: (CAN1_L, C12) and (CAN1_H, D12)

I would expect the channel at [(CAN2_L, C13) and (CAN2_H, D13)] and the channel at [(SBC_CAN_L, C11) and (SBC_CAN_H, D11)] to also work. So far, I have not been able to make these other channels work.

Are these other CAN channels on the dev board known to work with Simulink?

 

 

 

0 项奖励
回复
0 回复数