Use segger J-link instead of openSDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use segger J-link instead of openSDA

1,875 Views
theopubben
Contributor I

Within simulink i can select a com port or openSDA to download code to the target. Is it possible to use a J-link from Segger for this purpose?

Thank you.

0 Kudos
Reply
1 Reply

1,614 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Theo, 

The Simulink can only download (for the moment) via UART type protocols. Hence you cannot use JTAG based protocols directly from Simulink - BUT - you may generate and built the application from Simulink and get the elf/mot/srec file associated with the application and downloaded via the J-link using an external debugger such as S32 Design Studio that support the JTAG based protocols.

Hope this helps!

Daniel

0 Kudos
Reply