Undefined function 'slsfnagctlr'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Undefined function 'slsfnagctlr'

Jump to solution
5,253 Views
brunotremblay
Contributor III

Hi,

I'm beginning to develop my master project on model-based design using a FRDM-KV31F board and will switch to the TWR-KV58F220M later. I’m using MATLAB R2018b with all the required products specified on the MBD NXP site.

 

To start, I ‘tried some examples that came with the Kinetis MCToolbox and nothing works. On every example, I get :

 

Undefined function 'slsfnagctlr' for input arguments of type 'char'.

 

As mentioned in another post, old version of the Motor Control Toolbox don’t support the latest version of MATLAB.

Is there a fix on that problem?

 

Bruno T.

0 Kudos
Reply
1 Solution
4,845 Views
constantinrazva
NXP Employee
NXP Employee

Hello brunotremblay‌,

For newer versions of MATLAB you need to get the patch available here.

Kind regards,

Razvan.

View solution in original post

0 Kudos
Reply
4 Replies
4,845 Views
brunotremblay
Contributor III

Hello Constantin,

The patch works fine. Thanks for the help.

Now I'm trying the ADC example and I get a strange message.

Compiler details : "C:\Freescale\KDS_v3\Toolchain\arm-none-eabi\bin/bin/arm-none-eabi-gcc" -c -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -g -gstrict-dwarf -DARM_MATH_CM4 -o SetupFiles -DCPU_MK22FN512VDC12 -DDEBUG -I. -I.. -IC:\Users\Bruno\Documents\MATLAB\MCToolbox\mctbx_Kinetis\mctbx_kv3xf\Examples -IC:\Users\Bruno\Documents\MATLAB\MCToolbox\mctbx_Kinetis\mctbx_kv3xf\Examples\kv3xf_adc_mcd_rtw -IC:\PROGRA~1\MATLAB\R2018b\extern\include -IC:\PROGRA~1\MATLAB\R2018b\simulink\include -IC:\PROGRA~1\MATLAB\R2018b\rtw\c\src -IC:\PROGRA~1\MATLAB\R2018b\rtw\c\src\ext_mode\common -IC:\PROGRA~1\MATLAB\R2018b\rtw\c\ert -I"C:\Program Files\MATLAB\R2018b\simulink\include" -I"C:\Program Files\MATLAB\R2018b\extern\include" -I"C:\Program Files\MATLAB\R2018b\rtw\c\src" -I"C:\Program Files\MATLAB\R2018b\rtw\c\libsrc" -I"C:\Program Files\MATLAB\R2018b\rtw\c\src\ext_mode\common" -I"C:\Program Files\MATLAB\R2018b\rtw\c\src\ext_mode\tcpip" -I"C:\Program Files\MATLAB\R2018b\rtw\c\src\ext_mode\serial" -I"C:\Program Files\MATLAB\R2018b\rtw\c\src\ext_mode\custom" -I"C:\Freescale\KDS_v3\Toolchain\arm-none-eabi\bin/arm-none-eabi/include" -I".\device" -I".\device\MK22F51212" -I"..\device" -I"..\device\MK22F51212" Assembler details : Building file startup_MK22F51212.o... "C:\Freescale\KDS_v3\Toolchain\arm-none-eabi\bin/bin/arm-none-eabi-as" -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -g -o startup_MK22F51212.o startup_MK22F51212.s Le chemin d'accès spécifié est introuvable. gmake: *** [startup_MK22F51212.o] Error 1
### Build procedure for model: 'kv3xf_adc' aborted due to an error. Error make_rtw: exception id RTW:buildProcess:fatalBuildError message Error(s) encountered while building "kv3xf_adc"
Do you know why the compiler try to compile for the MK22F51212 ?
Regards
Bruno
0 Kudos
Reply
4,845 Views
constantinrazva
NXP Employee
NXP Employee

Hello brunotremblay‌,

Can you run the following command in MATLAB terminal and share it's output?

getenv('GCC_ARM_TOOL')

And also this one?

mcd_find_kv_root

Kind regards,

Razvan.

0 Kudos
Reply
4,845 Views
brunotremblay
Contributor III

Hello Constantin Razvan Chivu,

The output is :

>> getenv('GCC_ARM_TOOL')

ans =

'C:\Freescale\KDS_v3\Toolchain\arm-none-eabi\bin'

>> mcd_find_kv_root

ans =

'C:\Users\Bruno\Documents\MATLAB\MCToolbox\mctbx_Kinetis'

Regards,

Bruno

0 Kudos
Reply
4,846 Views
constantinrazva
NXP Employee
NXP Employee

Hello brunotremblay‌,

For newer versions of MATLAB you need to get the patch available here.

Kind regards,

Razvan.

0 Kudos
Reply